0614CT1701

MasterPacT MTZ Integration with Smart Systems

Ethernet-Ready Smart Systems

Ethernet-ready Smart Systems enable electrical distribution control and expertise. “Protect”, “Measure”, and “Connect” are the three pillars of this technology.

  1. Connect
    Give a voice to the equipment.
    Secured Ethernet network data transmission is part of the design of protection and metering devices.

  2. Measure
    Keep a close eye on energy flows.
    The electrical equipment captures building-related data, by gathering it from the critical protection and metering components.

  3. Protect
    Electrical protection is at the core of Smart Systems.
    High-performance technology is built into every circuit breaker.

  4. Act
    Future savings, peace-of-mind
    Access to Smart System status and values is essential for taking advantages of monitoring and management services, locally or remotely.

Future Savings and Peace-of-Mind

Access Smart System status and values to take advantages of monitoring and management services, locally or remotely.

Access large, non-critical buildings with EcoStruxure Building and with EcoStruxure Energy Expert.

Access Small/Medium Buildings
with FDM128, Com’X™ 510, IFE, EcoStruxure Facility Expert

Day-to-Day Energy Management

Power availability, Power quality, Energy performance

For simply dealing with building user’s needs and energy constraints.

EcoStruxure Building Management provides electrical management, monitoring and energy accounting.

EcoStruxure Power Monitoring Expert (software for PC) collects Smart Systems values to provide expert analysis.

Access Large, Non-Critical Buildings with EcoStruxure Building
and EcoStruxure Energy Expert

For dealing with building user’s needs and energy constraints. EcoStruxure Building Management provides electrical management, monitoring and energy accounting.

Access Large, Critical Buildings
with EcoStruxure Power Monitoring Expert

EcoStruxure Power Monitoring Expert

http://pmedemo.biz/web/
ID: demo & Password: demo

Energy decisions are often crucial in large critical buildings.

EcoStruxure Power Monitoring Expert PC software collects Smart System values to provide expert analysis.

MicroLogic Control Unit and Enerlin'X™ Breaker Digital System

General Architecture

Ethernet has become the universal link between electrical equipment, computers and communicating devices inside buildings. The large amount of information which can be transferred makes the connection of the Enerlin'X Breaker Digital System to cloud-hosted and web-based services of Schneider Electric a reality.

MicroLogic X control units and interfaces offers multiple communication channels:

  • Connection to an Ethernet network through either an EIFE or an IFE interface module. The EIFE and IFE modules are connected to the MicroLogic X control unit by means of a ULP port and a prefabricated ULP cord. The EIFE is dedicated to drawout circuit breakers.

  • Connection to a Modbus SL (RTU) RS 485 bus is through an IFM interface module. The IFM module is connected to the MicroLogic X control unit by means of a ULP port and a prefabricated ULP cord.

  • Communication with a smartphone via a wireless powered Bluetooth channel or a self-powered NFC channel.

  • Communication with a PC via a USB port.

  • Connection to Internet-based servers or cloud platform. The connection to Internet can be performed through a Com'X module connected to internal Ethernet network. In addition MicroLogic X offers a wireless proprietary connectivity interface for communication with a Com'X module.

Drawout Circuit Breaker

Fixed Circuit Breaker

To improve the capabilities of monitoring and control, one or two IO modules connected to the ULP bus can be associated to IFE, EIFE, and IFM modules.

The EIFE is designed to monitor the three positions of the drawout circuit breaker when inserted in its cradle:

  • Circuit breaker racked IN (CE contact).

  • Circuit breaker racked OUT (CD contact).

  • Circuit breaker in test position (CT contact).

  • No additional IO module is required to monitor these three positions.

The connection of an FDM128 display unit on the Ethernet internal bus is possible for any configuration.

The following control orders, information and data, are made available on Ethernet and Modbus SL (RTU):

  • Control orders:

    • MX diag&com shunt trip opening order

    • XF diag&com shunt close closing order

  • Events:

    • All the events logged in the MicroLogic X control unit event logbooks

  • Status indications:

    • ON/OFF O/F

    • Spring charged CH

    • Ready to close

    • Overcurrent trip SDE

    • Connected / disconnected / test position CE/CD/CT

  • Measurements

    • Instantaneous measurement information

    • Averaged measurement information

    • Max/Min values

    • Energy metering

    • Power quality...

  • Operating assistance:

    • Protection settings and alarm

    • Histories

    • Maintenance indicators

  • Availability:

    • Access control by password, to be initialized by the user

MicroLogic X Control Unit in Enerlin'X Digital Systems

Confidentiality

  • Bluetooth Smart technology with wireless encrypted (AES-128) communication (IEEE 802.15.1).

  • Proprietary connectivity with wireless encrypted (AES-128) internal communication (IEEE 802.15.4).

  • NFC operates in very short range (a few centimeters).

  • Pairing method and encryption is compliant with NIST 800-121.

Integrity

  • Only Schneider Electric-signed firmware can be installed on the MicroLogic X control unit.

  • Only Schneider Electric-signed digital modules can be installed on the MicroLogic X control unit.

  • Only Schneider Electric-signed ULP modules can be installed on an IMU.

Availability

  • Access control done by password. To be initialized by the user to change the default values.

  • Restricted USB usage for communication profile only (no mass storage).

MicroLogic X control units can be incorporated in Enerlin'X digital system using EIFE and IFE interface modules. Enerlin’X provides a simple and reliable link to local LCD displays and expert applications over Ethernet.

It makes available on Ethernet most of the information collected in the circuit breakers and other electrical devices installed in a low voltage electrical equipment: Status, measurements, counters and alarms etc.

System Security

Operational security is important for electrical installations when it comes to local and remote interaction. Confidentiality, integrity and availability (also known as the AIC triangle) is a model designed to guide policies for information security within an organization and these elements are considered as the three crucial components of security.

In this context, confidentiality is provided by rules that limit access to information (equivalent to privacy), integrity means the information is trustworthy and accurate, and availability means there is access to the information by authorized people.

Bluetooth Smart Connectivity

MicroLogic X control units are equipped with Bluetooth 4.0 Smart wireless communication which allows a connection with a smartphone equipped with the same technology. Bluetooth Smart complies with the IEEE 802.15.1 standard.

NFC Connectivity

MicroLogic X control units are equipped with near field communication (NFC), which allows data exchange with a smartphone equipped with the same technology and follow the standard ISO/IEC 15693-3.

Proprietary Connectivity

MicroLogic X control unit are equipped with a proprietary connectivity means based on IEEE 802.15.4 standard which allows a connection with a Com'X module.

ULP Connectivity

ULP is a fast communication link dedicated to circuit breaker monitoring and control. It connects the circuit breaker to an Ethernet interface or an IO module. ULP operates at a speed of 1 Mb/s and is plug & play.

Ethernet Connectivity

Ethernet is a data link and physical layer protocol complying with the IEEE 802.3 standard. It operates at a speed of 10, 100 or 1000 Mbps. The maximum length of Ethernet cable between two devices is 100 m (328 ft.).

IFE and EIFE Ethernet interfaces can be connected to a PC, a laptop or a PLC over Ethernet.

The IFE Ethernet switchboard server provides a Modbus TCP/IP gateway over Ethernet to enable Modbus TCP communication from a Modbus TCP master to any Modbus slave devices connected to it. The maximum active Modbus TCP client connection is twelve.

IFE and EIFE Ethernet interfaces have an embedded web server (web page).

Modbus Connectivity

Modbus SL (RTU) is a communication protocol widely used in industrial networks. It operates according to a “primary-secondary” mode, where the secondary communicates one at a time with the primary. This is an RS 485 open bus on which communicating Modbus devices are connected. All types of PLCs and microcomputers may be connected on to the bus.

The maximum number of devices that may be connected to a bus depends on the type of devices, the baud rate (19200 is recommended), the volume of data exchanged, and the expected response time. The RS 485 physical layer offers up to 32 connection points on the bus (1 master, 31 slaves).

Maximum recommended length for Modbus SL (RTU) bus is 1200 m (3940 ft.).

Digitized Electrical Equipment Architecture Example

Enerlin'X Digital Devices for Connection and Monitoring

Enerlin'X Digital Devices for MasterPacT MTZ Circuit Breaker Connection and Monitoring

Name

Function

Protocol

Bin. Input

Analog. Input

Bin. Output

Cat. No.

To Device

To Server

Com'X 210
24 Vdc supply)

Energy Data Logger with Ethernet Gateway Function*

Modbus SL (RTU) & TCP/IP

Web Services

6

2

EBX210

Com'X 510

Ethernet Server with Ethernet Gateway Function*

Modbus SL (RTU) & TCP/IP

Web Services

6

2

EBX510

FDM128

Ethernet LCD color Touch Display

Modbus TCP/IP

LV434128

EIFE

Embedded Ethernet Interface*

ULP

Modbus TCP/IP

LV851001SP

IFE Switchboard Server

Ethernet Interface & Gateway*

ULP Modbus SL (RTU) & TCP/IP

Modbus TCP/IP

LV434002

IFE Interface

Ethernet interface for circuit breakers

ULP

Modbus TCP/IP

LV434001

IO

Input/Output Application Module for Circuit Breaker

ULP

6

1

3

LV434063

IFM interface

Modbus interface for circuit breakers

ULP

Modbus SL (RTU)

LV434000

    EIFO and I/O modules

EIFE Embedded Ethernet module full spare part kit for MTZ1-drawout

         

LV851100SP

    EIFO and I/O modules

EIFE Embedded Ethernet module full spare part kit for MTZ2/3-drawout

         

LV851200SP

    EIFO and I/O modules

EIFE Embedded Ethernet Spare Part stand-alone module for MTZ1/2/3-drawout

         

LV851001SP

    EIFO and I/O modules

Ethernet interface LV breaker

         

LV434001

    EIFO and I/O modules

Ethernet interface for LV breakers and gateway

         

LV434002

    EIFO and I/O modules

I/O application module

         

LV434063

    EIFO and I/O modules

EIFE Wire Accessories spare part kit for MTZ1-drawout

         

LV851120SP

    EIFO and I/O modules

EIFE Wire Accessories spare part kit for MTZ2/3-drawout

         

LV851220SP

    Ethernet display module

Front display module FDM128

         

LV434128

   

EIFE

Embedded Ethernet interface for LV circuit breaker

       

LV851100SP

   

IFE

Ethernet interface LV breaker

       

LV434010

 

Ethernet interface for LV breakers and gateway

       

LV434011

   

IO Application Module

IO module for LV circuit breakers

       

LV434063

Communication Options

EIFE

Embedded Ethernet module full spare part kit for MTZ2/3 drawout

LV851200SP

Embedded Ethernet spare part module MTZ1/2/3 drawout

LV851001SP

IFE

Ethernet interface LV breaker

LV434010

Ethernet interface for LV breakers and gateway

LV434011

Microswitches for MTZ2/3

LV847905SP

EIFE Accessories spare part kit for MTZ2/3

LV851220SP

I/O application module

LV434063

Ethernet display module

Electrical Equipment front display module FDM128 LV434128

LV434128

Enerlin'X Digital System Commissioning and Maintenance Tools

Plug and play commissioning tools provide added value to system builders as their panels can be functionally checked before delivery.

EcoStruxure Power Commission Software allows:

  • Setting up and testing electrical equipment.

  • Installing digital modules.

  • Reduced commissioning time and sped-up factory acceptance tests (FAT) and site acceptance tests (SAT).

  • Improved preventive maintenance work.

Smart System with Enerlin'X Digital Devices Example

MasterPacT MTZ Communication Architecture

ULP Wiring system

The wiring system is designed for low-voltage power electrical equipment. Installation requires no tools or special skills.

The prefabricated wiring supports both data transmission and power supply for the communications modules associated with MicroLogic X control units.

ULP System

ULP system is a fast communication link dedicated to circuit breaker monitoring and control.

It is well adapted to severe environments.

A choice of cables with different lengths is provided for the connection of the ULP port to EIFE, IFE or IO modules.

EIFE / IFE Interfaces

EIFE / IFE interfaces provide an IP address to any circuit breaker fitted with an ULP port.

The EIFE / IFE interfaces make all available data from the circuit breaker accessible from an Ethernet compatible display (FDM128), a PC with common browser, or a Modbus TCP/IP client.

EIFE / IFE interfaces generate their own web pages.

IO Application Module

The IO module is dedicated to circuit breakers with a ULP link.

It may maintain:

  • Control of the circuit breaker.

  • Control of applications around the circuit breaker such as the cooling system, load control, lighting, and pulse metering acquisition.

MTZ Drawout Circuit Breaker

MTZ Fixed Circuit Breaker

MTZ Fixed Circuit Breaker Without IO Module

MTZ Fixed Circuit Breaker with Additional IO Module

Note: For every MasterPacT MTZ circuit breaker the 24 Vdc supply of all the associated interface modules (ULP port, IFE, IFM, IO) must be delivered from the same 24 Vdc power supply.

Smart System Components

Smart System ULP Interface Module

In MasterPacT MTZ circuit breakers, an internal communication protocol (ULP port) is embedded in the MicroLogic X control unit (a BCM module is not needed), as well as the microswitch contacts necessary to obtain circuit breaker status information (OF, SDE, PF, CH).

MasterPacT MTZ Fixed Circuit Breaker

MasterPacT MTZ Drawout Circuit Breaker

NOTE: MasterPacT MTZ switches have no communication capabilities. They are not compatible with any communication architecture.

MasterPacT MTZ ULP Port

Depending on the type of the device (MasterPacT MTZ1, MTZ2, MTZ3, fixed or drawout version), the ULP port and its corresponding wiring kit is supplied as standard or as an option.

ULP Port Versions

   

Part Number

 

MTZ1 Fixed

 

LV850063SP

 

MTZ1/2/3Fixed

  .

LV850061SP

Optional

MTZ1 Drawout

 

LV850064SP

Optional

MTZ2/3 Drawout

 

LV850062SP

Standard

ULP wiring accessories [1]

Breaker ULP cord L = 0.35 m

LV434195

 

Breaker ULP cord L = 1.3 m

LV434196

 

Breaker ULP cord L = 3 m

LV434197

 

5 RJ45 connectors female/female

TRV00870

 

10 ULP line terminators

TRV00880

 

10 RJ45/RJ45 male cord L = 0.3 m

TRV00803

 

10 RJ45/RJ45 male cord L = 0.6 m

TRV00806

 

5 RJ45/RJ45 male cord L = 1 m

TRV00810

 

5 RJ45/RJ45 male cord L = 2 m

TRV00820

 

5 RJ45/RJ45 male cord L = 3 m

TRV00830

 

1 RJ45/RJ45 male cord L = 5 m

TRV00850

 

Communication Option Spare Parts

Catalog Number

ULP port modules

ULP port - for MasterPacT MTZ2/3 - fixed

LV850061SP

ULP port - for MasterPacT MTZ2/3 - drawout

LV850056SP

Monitoring and Control Spare Parts

Catalog Number

ULP wiring accessories *

Breaker ULP cord L = 0.35 m

LV434195

Breaker ULP cord L = 1.3 m

LV434196

Breaker ULP cord L = 3 m

LV434197

10 Modbus line terminators

VW3A8306DRC*

5 RJ45 connectors female/female

TRV00870

10 ULP line terminators

TRV00880

10 RJ45/RJ45 male cord L = 0.3 m

TRV00803

10 RJ45/RJ45 male cord L = 0.6 m

TRV00806

5 RJ45/RJ45 male cord L = 1 m

TRV00810

5 RJ45/RJ45 male cord L = 2 m

TRV00820

5 RJ45/RJ45 male cord L = 3 m

TRV00830

1 RJ45/RJ45 male cord L = 5 m

TRV00850

Use the ULP port and its corresponding wiring kit to:

  • Interconnect the MicroLogic X control unit with EIFE, IFE and IO modules.

  • Supply power to the control unit and the EIFE module.

  • Integrate the ULP bus line termination.

Note:

  • Possible connection of an IO module on the RJ45 ULP connector.

  • When the ULP port is installed the 24 Vdc power supply shall be disconnected from the terminals F1/F2 of the control unit.

  • The connection of the +/- of the power supply either on terminals F1/F2 of MicroLogic X control unit or on the +/- terminals of the ULP port must be strictly respected. Crossing the polarities may damage the device.

  • For every MasterPacT MTZ circuit breaker the 24 Vdc supply of all the associated interface modules (ULP port, IFE, IFM, IO) must be delivered from the same 24 Vdc power supply.

Smart System EIFE Embedded Ethernet Interface

EIFE Embedded Ethernet Interface Description

EIFE Embedded Ethernet Interface

Introduction

The EIFE embedded Ethernet interface module enables drawout MasterPacT MTZ circuit breakers to be connected to an Ethernet network.

It provides digital access to the data delivered by the MasterPacT’s MicroLogic X control unit. In addition it monitors the three positions of the circuit breaker when inserted in its cradle:

  • Circuit breaker racked IN.

  • Circuit breaker racked OUT.

  • Circuit breaker in test position.

Provides an Ethernet access to a single drawout MasterPacT MTZ circuit breaker.

Function

One circuit breaker is connected to the EIFE interface via its ULP port.

EIFE Interface Features

  • Dual 10/100 Mbps Ethernet port for simple daisy chain connection.

  • Device profile web service for discovery of the EIFE interface on the LAN.

  • Ethernet interface for drawout MasterPacT circuit breakers.

  • Embedded set-up web pages.

  • Embedded monitoring web pages.

  • Embedded control web pages.

  • Cradle status management (CE, CD, CT).

  • Built-in e-mail alarm notification.

  • RBAC (Role Base Access Control).

Mounting

The EIFE interface is mounted on the cradle of the drawout circuit breaker. There are two types of dedicated EIFE ULP cable, one for MasterPacT MTZ1 devices and one for MasterPacT MTZ2/MTZ3 devices.

24 Vdc Power Supply

The EIFE power supply is provided by the ULP port through the dedicated EIFE ULP cable.

EIFE Interface Firmware Update

The firmware can be updated using EcoStruxure Power Commission Software.

Required Circuit Breaker Communication Accessory

The connection to the EIFE interface requires an ULP communication port on the cradle of the drawout MasterPacT MTZ circuit breakers.

EIFE Mounting and Cabling

EIFE General Characteristics

Environmental Characteristics

Conforming to standards

IEC 60947-2, UL489, CSA C22.2 n°5

Certification

CE, EAC

Ambient temperature

storage

-40 to +85°C (-40 to +185°F)

operation

-25 to +70°C (-13 to +158°F)

Relative humidity

5 - 85%

Level of pollution

Level 3

Protective treatment

ULV0 conforming to IEC/EN 60068-2-30

Mechanical Characteristics

Shock resistance

As the EIFE is mounted on the circuit breaker it complies with its mechanical characteristics

Resistance to sinusoidal vibrations

Electrical Characteristics

Consumption

250 mA at 24 Vdc

Resistance to electrostatic discharge

  • 8 kV air discharge

  • 6 kV contact discharge

Immunity to radiated fields

IEC/EN 61000-4-3: 20 V/m

Immunity to fast transient perturbations

IEC/EN 61000-4-4: 2 kV

Immunity to surges

IEC/EN 61000-4-5: 2 kV common mode

Immunity to conducted radio frequency field

IEC/EN 61000-4-6: 10 V

Physical Characteristics

Dimensions

51 x 51 x 52.5 mm (2.07 in.)

Mounting

Circuit breaker DIN rail of MTZ1 & MTZ2/MTZ3

Weight

75 g (2.65 oz.) EIFE alone

Degree of protection of the installed module

  • IP20 for connectors

  • IP30 for other areas

Connections

  • RJ45 for Ethernet

  • Industrial USB connector for ULP

Smart System IFE Ethernet Interface

IFE Interface, IFE Switchboard Server Description

IFE Interface LV434001

IFE Switchboard Server LV434002

Introduction

The IFE interface and the IFE switchboard server enable LV circuit breakers to be connected to an Ethernet network.

  • The IFE switchboard server incorporates a Modbus gateway.

  • The IFE interface and IFE switchboard server are both equipped with two ULP ports and two Ethernet ports.

  • The IFE switchboard server is equipped with a Modbus RS 485 serial connection.

MasterPacT or PowerPacT™ circuit breakers can be connected to an IFE interface and to an IFE switchboard server:

IFE Interface: ref. LV434001

Provides an Ethernet access to a single LV circuit breaker. The MasterPacT MTZ circuit breaker is connected to the IFE interface via its ULP port and a prefabricated ULP cord *.

IFE Switchboard Server: ref. LV434002

Provides an Ethernet access to one or several LV circuit breakers. It allows to interface to Ethernet:

  • One single circuit breaker connected to the IFE interface via its ULP port and a prefabricated ULP cord.

  • Up to 12 PowerPacT circuit breakers connected through the modbus serial line interface.

Each PowerPacT device is connected to Modbus by means of a dedicated IFM interface module performing the ULP/Modbus conversion.

The connection between each PowerPacT device and its associated IFM interface is made using a prefabricated ULP cord connected to ULP ports.

IFE Interface, IFE Switchboard Server

  • Dual 10/100 Mbps Ethernet port for simple daisy chain connection.

  • Device profile web service for discovery of the IFE interface and IFE switchboard server on the LAN.

  • ULP compliant for localization of the IFE interface in the electrical equipment.

  • Ethernet interface for MasterPacT and PowerPacT circuit breakers.

  • Gateway for Modbus-SL (RTU) connected devices (IFE switchboard server only).

  • Embedded set-up web pages.

  • Embedded monitoring web pages.

  • Embedded control web pages.

  • Built-in e-mail alarm notification.

  • Internal real-time clock with battery back-up.

  • RBAC (Role Base Access Control).

Mounting

The IFE interface and the IFE switchboard server are DIN rail mounted devices.

A stacking accessory enables the user to connect several IFMs (ULP to Modbus serial line interfaces) to an IFE switchboard server without additional wiring.

24 Vdc power supply

Supply the IFE interface and the IFE switchboard with either a 24 Vdc AD or with a 24 Vdc ABL8 RPS power supply.

The IFMs stacked to an IFE switchboard server are supplied by the IFE, thus it is not necessary to supply them separately.

NOTE: The connection of the +/- of the power supply on +/- terminals of the IFE device must be strictly respected. Crossing the polarities may damage the device.

IFE Interface, IFE Switchboard Server Firmware Update

The firmware can be updated using the Ecoreach software.

Required Circuit Breaker Communication Modules

The connection to an IFE interface or to an IFE switchboard server requires ULP communication ports. Every MasterPacT MTZ fixed-type circuit breaker is equipped with a ULP port connected to its associated IFE Ethernet interface module by a prefabricated ULP cord. The IFE Ethernet interface modules are equipped with two ULP RJ45 connectors. When one is not used, it must be closed with a ULP terminator.

IFE Characteristics

IFE Web Page Description

Monitoring Web Page:

  • Real time data

  • Device logging.

Control Web Page:

  • Single device control.

Diagnostics Web Page:

  • Statistics

  • Device information

  • IMU information

  • Read device registers

  • Communication check.

Maintenance Web Page:

  • Maintenance log

  • Maintenance counters.

Setup Web Page:

  • Device localization/name

  • Ethernet configuration (dual port)

  • IP configuration

  • Modbus TCP/IP filtering

  • Serial port

  • Date and time

  • E-mail server configuration

  • Alarms to be e-mailed

  • Device list

  • Device logging

  • Device log export

  • SNMP parameters

  • Documentation links

  • Preferences

  • Advanced services control

  • User accounts

  • Web page access.

IFE General Characteristics

General Characteristics

Environmental Characteristics

Conforming to standards

IEC 60950, UL 60950

Certification

cULus, CE, EAC

Ambient temperature

storage

-40 to +85°C (-40 to +185°F)

operation

-25 to +70°C (-13 to +158°F)

Relative humidity

5 - 85%

Level of pollution

Level 3

Protective treatment

ULV0 conforming to IEC/EN 60068-2-30

Mechanical Characteristics

Shock resistance

Conforming to IEC/EN 60068-2-27 15 g / 11 ms, 1/2 sinusoidal

Resistance to sinusoidal vibrations

Conforming to IEC/EN 60068-2-6 5 Hz < f < 8.4 Hz

Electrical Characteristics

Consumption

150 mA at 24 Vdc

Resistance to electrostatic discharge

IEC/EN 61000-4-2:

  • 8 kV air discharge

  • 6 kV contact discharge

Immunity to radiated fields

IEC/EN 61000-4-3: 10 V/m

Immunity to fast transient perturbations

IEC/EN 61000-4-4: 2 kV

Immunity to surges

IEC/EN 61000-4-5: 2 kV common mode

Immunity to conducted radio frequency field

IEC/EN 61000-4-6: 10 V

Physical Characteristics

Dimensions

72 x 105 x 71 mm (2.83 x 4.13 x 2.79 in.)

Mounting

DIN rail

Weight

182.5 g (0.41 lb)

Degree of protection of the installed IO module

  • On the front panel (wall mounted enclosure): IP4x

  • Connectors: IP2x

  • Other parts: IP3x

Connections

Screw type terminal blocks

Smart System IO Application Module

IO Application Module Description

IO Application Module

The IO input/output application module for LV circuit breakers is one of the components of ULP architecture. Built in functions and applications enhance control and monitoring needs.

ULP system architecture including IO modules can be built without any restrictions using a wide range of circuit breakers:

  • MasterPacT MTZ1/MTZ2/MTZ3/NT/NW circuit breakers

  • PowerPacT P- and R-frame circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

The IO application module is compliant with the ULP system specifications.
Two IO application modules can be connected to each circuit breaker on the same IMU.

IO Input/Output Interface for LV Circuit Breaker Resources

The IO application module resources are:

  • Six self-powered digital inputs for either NO and NC dry contact or pulse counter.

  • Three bistable relay digital outputs (5 A maximum).

  • One analog input for a Pt100 temperature sensor.

 

Pre-Defined Applications

Use the nine-position rotary switch on the front of the IO module to select a pre-defined applications. Each position is assigned to a predefined application except position 9, which allows the user to define a specific application using the EcoStruxure Power Commission Software. The switch is factory set to predefined application 1.

For each pre-defined application the input/output assignment and the wiring diagram are predefined. No additional setting with the customer engineering tool is required.

The IO module and other resources not assigned to the predefined applications are free for user specific applications.

User Applications

The user applications with the corresponding resources are defined by means of the EcoStruxure Power Commission Software. They use the resources not assigned to the predefined applications. User applications can be used for:

  • Protection improvement

  • Circuit breaker control

  • Motor control

  • Energy management

  • Monitoring

24 Vdc Power Supply

The IO module must be supplied with either a 24 Vdc AD or with a 24 Vdc ABL8 RPS power supply.

NOTE: The +/- of the power supply must be connected to the +/- terminals of the IO module. Crossing the polarities may damage the device.

Mounting

The IO module is a DIN rail mounted device.

Setting IO Application Module Locking Pad

The setting locking pad on the front panel of the IO module enables/disables the setting of the IO module using the EcoStruxure Power Commission Software.

IO Application Module Characteristics


General Characteristics

Environmental Characteristics

Conforming to standards

IEC 60950, UL 60950

Certification

CE, cULus, EAC

Ambient temperature

storage

-40 to +85°C (-40 to +185°F)

operation

-25 to +70°C (-13 to +158°F)

Relative humidity

5 - 85%

Level of pollution

Level 3

Protective treatment

ULV0 conforming to IEC/EN 60068-2-30

Mechanical Characteristics

Shock resistance

Conforming to IEC/EN 60068-2-27: 15 g / 11 ms, 1/2 sinusoidal

Resistance to sinusoidal vibrations

Conforming to IEC/EN 60068-2-6: 5 Hz < f < 8.4 Hz

Electrical Characteristics

Consumption

165 mA at 24 Vdc

Resistance to electrostatic discharge

IEC/EN 61000-4-2: 8 kV air discharge, 6 kV contact discharge

Immunity to radiated fields

IEC/EN 61000-4-3: 10 V/m

Immunity to fast transient perturbations

IEC/EN 61000-4-4: 2 kV

Immunity to surges

IEC/EN 61000-4-5: 2 kV common mode

Immunity to conducted radio frequency field

IEC/EN 61000-4-6: 10 V

Physical Characteristics

Dimensions

71.7 x 116 x 70.6 mm (2.82 x 4.57 x 2.78 in.)

Mounting

DIN rail

Weight

229.5 g (0.51 lb)

Degree of protection of the installed IO application module

On the front panel (wall mounted enclosure): IP4x

IO parts: IP3x

Connectors: IP2x

Connections

Screw type terminal blocks

Input and Output Characteristics

Digital Inputs

Digital input type

Self powered digital input with current limitations as per IEC 61131-2 type 2 standards (7 mA)

Input limit values at state 1 (close)

19.8–25.2 Vdc, 6.1 - 8.8 mA

Input limit values at state 0 (open)

0–19.8 Vdc, 0 mA

Maximum cable length

10 m (33 ft.)

NOTE: For a length greater than 10 m (33 ft.) and up to 300 m (984 ft.), it is mandatory to use a shielded twisted cable. The shield cable is connected to the IO functional ground of the IO application module.

Digital Outputs

Digital output type

Bistable relay

Rated voltage

250 Vac maximum */ 30 Vdc

Rated carry current

5 A

Contact resistance

30 mΩ

Maximum operating frequency

18,000 Operations/hr (Mechanical)

1800 Operations/hr (Electrical)

Digital output relay protection by an external fuse

External fuse of 5 A or less

Maximum cable length

10 m (33 ft.)

Analog Inputs

IO application module analog input can be connected to a Pt100 temperature sensor.

Range

-30 to 200°C

-22 to 392°F

Accuracy

±2°C from -30 to 20°C

±3.6°F from -22 to 68°F

±1°C from 20 to 140°C

±1.8°F from 68 to 284°F

±2°C from 140 to 200°C

±3.6°F from 284 to 392°F

Refresh interval

5 s

5 s

Smart System FDM128 Display Unit

MicroLogic X control units measurement capabilities come into full play with the FDM128 display unit. It connects to Ethernet communication via RJ45 port and displays MicroLogic X control unit information.

FDM128 display.

General view

Role base access control

Editing devices

General setting

FDM128 Display

The FDM128 is an intelligent Ethernet touch screen. It collects the data from devices via the Ethernet network. It is designed to manage up to eight devices such as:

  • MasterPacT MTZ1,MTZ2, MTZ3, NT, and NW circuit breakers

  • PowerPacT P- and R-frame circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

The FDM128 switchboard display unit can be connected to a MicroLogic X control unit via an IFE or an EIFE interface module. It is easy to use and requires no special software or programming.

The FDM128 has a large screen which requires little depth for mounting or installation. The anti-glare graphic screen has a backlight for easy reading even under poor ambient lighting and at sharp angles.

Display of MicroLogic X Measurements and Trips

The FDM128 is intended to display the MicroLogic X control unit measurements, trips and operating information.

  • The FDM128 cannot be used to modify the protection settings.

  • Measurements are easily accessed via a menu.

  • Trips are automatically displayed.

  • A pop-up window displays the time-stamped description of the trip.

Status Indications

When the circuit breaker is equipped with the Command Module, the FDM128 display can also be used to view circuit breaker status conditions:

  • ON/OFF (OF)

  • Spring loaded (CH)

  • Overcurrent trip indication (overload, short circuit, ground fault) (SDE)

  • Cradle management with EIFE (CE, CD, CT)

Remote Control

When the circuit breaker is equipped with communicating XF, MX, or MN devices, the FDM128 display can also be used to control the circuit breaker (initiation of open/close commands).

Main Characteristics

  • 115.2 x 86.4 mm (4.54 x 3.50 in.) with 5.7 in. QVGA display 320 x 240 pixels

  • Color TFT LCD, LED backlight

  • Wide viewing angle: vertical ± 80°, horizontal ± 70°

  • High resolution: excellent reading of graphic symbols

  • Operating temperature range -10°C to +55°C (-14°F to +131°F)

  • CE / UL / CSA marking

  • 24 Vdc power supply

  • Consumption ≤ 6.8 W

  • One RJ45 Ethernet jack

Mounting and Protection

  • The FDM128 is easily installed in electrical equipment.

  • Standard door hole Ø 22 mm (0.87 in.).

  • The FDM128 degree of protection is IP65.

Quick View

Measures

Alarm History

Control

Maintenance

FDM128 Main Menu

General view
Provides in one shot the information about the status of each monitored device

Role base access control
Allows management of logins and passwords.

Editing devices
Allows specification of the devices monitored by the FDM128.

Communication setting
Allows setting of the communication parameters.

General setting
Allows selection of the language and setting of the other parameters of FDM128

FDM128 Display Unit Sub Menus

Quick view

Provides access to five screens that display a summary of essential operating information (I, U, f, P, E, THD, circuit breaker On/off), and protection settings.

Measures

Displays all measurements (I, U, V, f, P, Q, S, E, THD, PF) with the corresponding min/max values.

Alarms history

Displays tripping and alarms histories.

Control

Displays the status of the devices (Open/Closed) and allows initiation of control commands (Open/Close/Reset)

Maintenance

Displays all circuit breaker condition indications and all the information generated by the diagnostic functions (number of operations, contact wear, operating time, internal temperature etc.)

Customer Engineering Tool: EcoStruxure Power Commission Software

EcoStruxure Power Commission Software

Definition

EcoStruxure Power Commission Software helps the user manage a project as part of the testing, site commissioning, and maintenance phases of the project life cycle.

With EcoStruxure Power Commission Software, electrical devices can be configured, tested and commissioned in the simplest way.

EcoStruxure Power Commission Software reduces the commissioning time of Smart Systems and supports the system during operation & maintenance.

EcoStruxure Power Commission Software offers valuable added features like automatic discovery of connected devices, performs communication tests, generates comprehensive reports, upgrades firmware etc.

Description

EcoStruxure Power Commission Software enables the user to perform the following actions for the devices and modules listed in the table below:

  • Create projects by device discovery.

  • Perform circuit breaker and communication tests and generate reports.

  • Configuration or settings download and upload for multiple devices.

  • Install digital modules.

  • Compare settings between the project (original settings) and device (current settings).

  • Generate comprehensive project reports.

  • Check system level firmware status and upgrade devices.

  • Secured repository of projects in Cloud.

  • Read information (alarms, measurements, parameters) & display diagnostic information.

  • Waveform capture.

USB and Ethernet Interfaces

EcoStruxure Power Commission Software provides access to MasterPacT MTZ devices through USB and Ethernet interfaces. The following table indicates the features that are accessible through each interface:

Features

USB

Ethernet

Protection/Alarm settings

Yes

Yes

Firmware upgrade

Yes

No

Digital modules installation

Yes

No

Device Checkup

Yes

Yes

IO Module Configuration

Yes

Yes

EcoStruxure Power Commission Software Key Features

Device Discovery:

EcoStruxure Power Commission Software helps the user to discover the communicating devices in electrical equipment either through Ethernet or a serial network. Once the devices are discovered, the user can add those devices to the project area.

Device settings:

EcoStruxure Power Commission Software helps the user to set the protection settings and the alarms of the MasterPacT MTZ devices including dual settings and IO module configuration.

Communication Test:

When a user has installed communicating devices in electrical equipment, EcoStruxure Power Commission Software offers the capability to test the communication network. Once a communication test is done, the user can generate a time stamped communication test report.

Reports

EcoStruxure Power Commission Software offers the following reports to the users

  • Circuit breaker and communication test reports

  • Comprehensive project report

  • Logs and trip history reports

Firmware Upgrade

EcoStruxure Power Commission Software offers a system compatibility check and firmware upgrade for the following devices.

  • MicroLogic X control units

  • EIFE / IFE / IFM

  • IO modules

Digital Modules Support

EcoStruxure Power Commission Software helps the user to buy digital modules which allows digital customization of the devices.

EcoStruxure Power Commission Software directs the user to the GoDigital platform to purchase digital modules.

After purchase, EcoStruxure Power Commission Software helps to install/uninstall the digital modules in the MicroLogic X control unit in a secured way.

Sharing with EcoStruxure Facility Expert

EcoStruxure Power Commission Software offers the chance to share project with Facility Expert. A digital logbook is then automatically created for the MasterPacT MTZ device.

EcoStruxure Power Commission Software Operations

Screen: Device Homepage

The user can connect to the device from the device home page and do the settings configuration, do a device check up, view maintenance information, upgrade the device with the latest firmware & install/uninstall digital modules.

Screen: General View

Through the welcome screen, a user can create a project, have access to devices and discover them.

The welcome screen allows the user to open reports to have view of his projects, to modify them, to check if they are synchronized with the cloud and if they are shared with EcoStrucxure Facility expert.

The user can change the language and have access to the help files and to device firmware baseline file.

Screen: Protections

Once the user clicks on configuration, this screen appears, through which the user can read/ write different settings and check the settings discrepancies.

The user can change the language and have access to the help files and to device firmware baseline file.

Screen: Measures

Once the user clicks on Device Checkup section from the device home page, this screen appears and the user can view the measurement parameters, IO status , Alarms logs, maintenance parameters etc.

Screen: Digital Modules

Once the user clicks on Digital modules, this screen appears and the user can buy the desired digital module specific to the device & install the digital module to the device.

Once the user clicks on configuration, this screen appears, through which the user can read/ write different settings and check the settings discrepancies.

Screen: Firmware Upgrades

Through the Firmware Upgrade screen, a user can check the compatibility of the firmware versions of the devices and modules connected and upgrade them when needed with the device firmware baseline file.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.