0614CT1701

MasterPacT MTZ Integration in Electrical Equipment

MasterPacT MTZ Electrical Equipment Operating Conditions

MasterPacT MTZ test conditions reproduce different customer environments, in accordance with product and installation standards and relevant maintenance operations * to maximize the product lifespan.

Selecting MasterPacT MTZ2 Circuit Breakers

Operating Conditions

MasterPacT MTZ devices are designed for specified operating conditions in terms of temperature, humidity, vibration, altitude, corrosion, and electromagnetic disturbances.

Beyond the limits defined here, the circuit breakers suffer accelerated aging that may rapidly result in equipment breakdowns.

Refer to the MasterPacT Maintenance Guide for additional information and consult Schneider Electric to confirm mechanical and electrical performances in severe conditions.

Examples of applications with severe operating conditions:

  • wind turbines

  • power frequency converters installed in the same electrical equipment or close to the MasterPacT circuit breaker

  • emergency generators

  • high vibration marine applications such as thrusters and anchor positioning systems

Safety of Operations

The front face of the MasterPacT MTZ device provides reinforced insulation (Class 2) according to IEC 60664-1. It allows Class 2 installation with circuit breaker control from outside.

Ambient Temperature

MasterPacT MTZ devices are designed to operate in ambient temperature between -25°C (-13°F) and +70°C (+158°F), providing that the temperature around the circuit breaker inside the enclosure does not exceed +70°C (+158°F). If this condition cannot be fulfilled, dedicated measures such as HVAC must be taken.

MasterPacT MTZ devices have successfully passed the tests defined by the following standards for extreme atmospheric conditions:

  • Dry cold at -40°C (-40°F) (IEC 60068-2-1)

  • Dry heat at +85°C (+185°F) (IEC 60068-2-2)

  • Damp heat (temperature +55°C (+131°F), relative humidity 95%)
    (IEC 60068-2-30)

MasterPacT MTZ Circuit Breakers Ambient Temperatures

Shipping & Storage

Installation & Commissioning

Inside the Electrical Equipment Containing the Circuit Breaker

Temperature

Relative Humidity

Temperature

Relative Humidity

Temperature

Relative Humidity

-40°C / +85°C
(-40°F / +185°F)

0 to 95%

-25°C / +70°C
(-13°F / +158°F)

0 to 95%

-25°C / +70°C
(-13°F / +158°F)*

0 to 95%

Vibration Tests

MasterPacT MTZ devices have successfully passed testing in compliance with IEC 60068-2-6 for the following vibration levels:

  • 2 to 13.2 Hz: amplitude ±1 mm

  • 13.2 to 100 Hz: constant acceleration 0.7 g

Vibration testing to these levels is required by merchant marine inspection organizations (such as Veritas, and Lloyd’s).

Industrial Environmental Atmospheric Conditions

MasterPacT MTZ devices have successfully passed the tests defined by IEC 60068-2-52 level 2: salt mist for extreme atmospheric conditions:

MasterPacT devices can operate in the industrial environments defined by standard IEC/EN 60947-1 (pollution degree up to 3).

It is nevertheless advised to check that the devices are installed in suitably cooled electrical equipment without excessive dust.

Profile

Pollutions

Active Substances

Corrosive industrial atmospheres

Category 3C3 compliant with IEC 60721-3-3

Sea salts

Compliant with IEC 60721-2-5

0.8 to 8 mg/(m2. day)
Average over the year

Mechanically active substances

Category 3S3 compliant with IEC 60721-3-3

Beyond these conditions, MasterPacT MTZ devices must be installed inside electrical equipment with an enclosure rating equal to or greater than a NEMA 13 rating.

Altitude

Altitude Correction Factors per ANSI C37.20.1 par. 7.1.4.1

Altitude

< 2000 m
(6600 ft.)

2600 m
(8500 ft.)

3900 m
(13,000 ft.)

Voltage

1.00

0.95

0.80

Current

1.00

0.99

0.96

Electromagnetic Disturbances

MasterPacT MTZ devices are protected against:

  • Overvoltages caused by devices that generate electromagnetic disturbances.

  • Overvoltages caused by atmospheric disturbances or by a distribution-system outage (for example, failure of a lighting system).

  • Devices emitting radio waves (radios, walkie-talkies, radar, etc.).

  • Electrostatic discharges produced by users.

MasterPacT MTZ devices have successfully passed the electromagnetic compatibility tests (EMC) defined by IEC/EN 60947-2, Annex F.

This testing reduces the chance of:

  • Nuisance tripping

  • Tripping times outside of published curves

Immunity: ability of a device to operate without damage in the presence of an electromagnetic disturbance.

Susceptibility: inability of a device to operate without damage in the presence of an electromagnetic disturbance.

Conducted interference: disturbances generated by the device and transmitted by the conductors (of power supply, signalling, or control) in the form of electrical voltage.

Radiated interference: disturbances generated by the device and radiated in the environment in the form of electromagnetic waves.

MasterPacT MTZ Electromagnetic Immunity

     

Electromagnetic Compatibility (EMC)

Standard

Level

Test Values Required by IEC 60947-2

Tested Extra EMC Performances

To Conducted Disturbances

Electrical fast transient/ burst
(EFBT/B)

IEC 61000-4-4

4 kV ; 5 kHz on poles and all AC supplies
2 kV ; 5 kHz on auxiliaries DC supply and signal ports

4 kV ; 5 kHz and 100 kHz on poles and all AC supplies
2 kV ; 5 kHz and 100 kHz on auxiliaries DC supply and signal ports

Surges

IEC 61000-4-5

4

4 kV CM, 2 kV DM on poles and AC supply > 100 V
2 kV CM, 1 kV DM on AC supply < 100 V

6.6 kV CM, 4.4 kV DM on poles.
4 kV CM, 2 kV DM on MX-XF-MN voltage releases for supply > 100 V.
2 kV CM, 1 kV DM on MX-XF-MN voltage releases for supply < 100 V.
2 kV CM, 1 kV DM on 24 V DC supply.
2 kV CM, on all signals ports.

Conducted disturbances induced by radio-frequency fields

IEC 61000-4-6

4

10 V CM; 0,15…80 MHz (with CDN)

20 V CM; 0.15...80 MHz

Voltage dips, voltage sags, voltage interruption (AC supply)

IEC 61000-4-11

40 % (10/12 cycles); 70 % (25/30 cycles); 80 % (250/300 cycles)
0 % (0.5 cycle); 0 % (1 cycle); 0 % (250/300 cycles)
External power supply problem:

  • 3 interruptions during 5 minutes;

  • switching-off time 30 s each case

Combined voltage and frequency variations

Conducted low frequency

IACS— E10 (§15)

  • AC: 50 Hz to 10 kHz ; 10 % of the rated voltage supply up to harmonic 15. Then reduction at 1% up to harmonic 100, min 3 V RMS.

  • DC: 50 Hz to10 kHz; Test voltage 10% of the maximum voltage supply 2 W.

Harmonics and Interharmonics including mains signalling at a.c. power ports

IEC 61000-4-13 3

3

AC supply of devices < 16 A

Immunity to conducted, common mode disturbances of main frequencies

IEC 61000-4-16

Only on pole accesses:
30-3 V; CM; 15-150 Hz; 3 V; CM; 150-1,5 kHz
3-30 V; CM; 1,5-15 kHz; 30 V; CM; 15-150 kHz

Oscillatory wave

IEC 61000-4-18

2,5 kV CM, 2,5 kV DM; 1 MHz

Voltage dips, voltage sags, voltage interruption (DC supply)

IEC 61000-4-29

40 % (10/12 cycles); 70 % (25/30 cycles)
0% (0,5 cycle); 0 % (50 ms); 0 % (250/300 cycles) variations on DC : U ±20%; 10 sec

External power supply problem:

  • 3 interruptions during 5 minutes;

  • switching-off time 30 s each case

Voltage continuous ±10%; Voltage cyclic variation 5%; Voltage ripple10%

40 % (10/12 cycles); 70 % (25/30 cycles)
0% (0,5 cycle); 0 % (50 ms); 0 % (250/300 cycles) variations on DC : U ±20%; 10 sec
External power supply problem:

  • 3 interruptions during 5 minutes;

  • switching-off time 30 s each case


Voltage continuous ±10%; Voltage cyclic variation 5%; Voltage ripple10%

To Radiated Disturbances

Electrostatic discharge IEC 61000-4-2

IEC 61000-4-2

3

8 kV air ; 8 kV contact

9,6 kV air ; 9,6 kV contact

IACS - E10

Radiated radio-frequency electromagnetic fields

IEC 61000-4-3

3

10 V/m ; 80 MHZ…1 GHz; 1.4…2 GHz
10 V/m ; 80 MHz…2 GHz
10 V/m ; 80 MHz…1 GHz; 3 V/m ; 1.4-2 GHz;
1 V/m 2-2.7 GHz

20 V/m; 80 MHZ…3 GHz

Power frequency magnetic fields

IEC 61000-4-8

400 A/m permanently

500 A/m permanently, 1000 A/m during 3 s

Impulse magnetic field

IEC 61000-4-9 5

5

1000 A/m (8/20 μs wave)

Oscillatory magnetic field

IEC 61000-4-10

100 A/m (100 kHz and 1 MHz)

MasterPacT MTZ Electromagnetic Emission

     

Electromagnetic Compatibility (EMC)

Standard

Level

Test values required by IEC 60947-2

To Conducted Disturbances

Limits for harmonic current emissions

IEC 61000-3-2 A

A

For Ie ≤ 16 A (0 to 2 kHz) and coils
240 Vac / 380 Vac

Conducted emission

CISPR 11/22

A

B (with external filters on MN/MX/XF Coils and with 24 Vdc external, please consult us)

B

B (with external filters on MN/MX/XF Coils and with 24 Vdc external, please consult us)

CISPR 16

A

To Radiated Disturbances

Radiated emission

CISPR 11/22
CISPR 16

B

EMC and ERM tests compliant with:

  • ETSI EN 300 328 and ERC Recommendation 70-03.

  • FCC CFR47 Part 15, Subpart B and C, RSS-210 Issue 8

  • ETSI EN 300 440-1 /-2

  • ETSI EN 302 291-1 /-2.

Directive RTTE -

  • Bluetooth technology (Low Energy and Modulation DSSS)

  • Proprietary connectivity

  • NFC (Near Field Communication)

MasterPacT MTZ Electrical Equipment Installation Rules

MasterPacT MTZ Device Installation

MasterPacT MTZ devices can be supplied either from the top or from the bottom without degrading performance, in order to facilitate connection when installed in electrical equipment.

Mounting the Circuit Breaker

The weight of the device must be distributed uniformly over a rigid mounting surface such as rails or a base plate.

This mounting plane must be perfectly flat (tolerance on support flatness:
2 mm [0.08 in.]).

Mounting the circuit breaker to a mounting plate that does not meet the flatness requirements could interfere with the correct operation of the circuit breaker.

MasterPacT MTZ devices can also be mounted on a vertical plane using special brackets.

Mounting on Rails

Mounting with Vertical Brackets

MasterPacT MTZ Position in Electrical Equipment

Only one position is authorized.

Electrical Equipment Partitions for MasterPacT MTZ Devices

Sufficient openings must be provided in partitions to maintain good air circulation around the circuit breaker. Any partition between upstream and downstream connections of the device must be made of non-magnetic material.

For high currents, 2500 A and above, the metal supports or barriers in the immediate vicinity of a conductor must be made of non-magnetic material [1].

Metal barriers [2] through which a conductor passes must not form a magnetic loop.

[1] Non-magnetic material

[2] Metal barriers

MasterPacT MTZ Electrical Equipment Busbars

Creating a magnetic loop around a conductor, (via the busbar support for example), must be strictly avoided.

To avoid this:

  • Either the busbar supports (A) and/or their mounting screws (B) must be made of non-magnetic materials.

  • Maintain minimum distances for control wires (C) and busbar (D).

A) Busbar supports

B) Busbar support screws

Door Interlock

Door Interlock (VPEC)

Mounted on the right or left-hand side of the cradle, this device inhibits opening of the cubicle door when the circuit breaker is in “connected” or “test” position.

If the circuit breaker is put in the “connected” position with the door open, the door may be closed without having to disconnect the circuit breaker.

Door Interlock Dimensions

Type

Dimensions

[1] mm (in.)

[2] mm (in.)

MTZ1 08-16 (3P)

135 (5.31)

168 (6.61)

MTZ1 08-16 (4P)

205 (8.07)

168 (6.61)

MTZ2 08-40 (3P)

215 (8.46)

215 (8.46)

MTZ2 08-40 (4P)

330 (12.99)

215 (8.46)

MTZ3 40-63 (3P)

660 (25.98)

215 (8.46)

MTZ3 40-63 (4P)

775 (30.51)

215 (8.46)

MTZ1

MTZ2 - MTZ3

Circuit Breaker in Connected or Test Position

Door cannot be opened

MTZ1 06-16

MTZ2 08-40

MTZ3 40-63

Type

Dimensions (mm)

A
mm (in.)

B
mm (in.)

MTZ1 08-16 (3P)

5 (0.197)

23 (0.906)

MTZ1 08-16 (4P)

5 (0.197)

23 (0.906)

MTZ2 08-40 (3P)

87 (3.43)

103 (4.063)

MTZ2 08-40 (4P)

87 (3.43)

103 (4.063)

MTZ3 40-63 (3P)

37 (1.46)

53 (2.09)

MTZ3 40-63 (4P)

37 (1.46)

53 (2.09)

Circuit Breaker in Disconnected Position

Door can be opened

Mounted on the right or left-hand side of the cradle, this device inhibits opening of the cubicle door when the circuit breaker is in the “connected” or “test” position.

It the circuit breaker is put in the “connected” position with the door open, the door may be closed without having to disconnect the circuit breaker.

MTZ1 06-16

MTZ2 08-40

MTZ3 40-63

Power Connection

MasterPacT MTZ Electrical Equipment Cable Connections

If cables are used for the power connections, their weight must not be applied to the circuit breaker power terminals, but must be supported by the panel structure.

For this, make the connections as follows:

  • Extend the device terminals using short bars designed and installed according to the recommendations for bar-type power connections (see figure below):

    • For a single cable, use solution [1].

    • For a multiple cables, use solution [2].

  • In all cases, follow the general rules for connections to busbars:

    • Position the cable lugs before inserting the bolts

      .
    • Firmly secure the cables to the framework [3].

Busbar Connections

Install with a maximum distance A between busbar to circuit breaker connection and the first busbar support or spacer with respect to the value of the prospective short-circuit current.

  • The busbars must be suitably adjusted so that the connection points are positioned on the power terminals before the bolts [4] are inserted.

  • The busbars weight must be supported by the busbar supports [5] that are solidly fixed to the electrical equipment framework and not by the circuit breaker power terminals.

Electrodynamic Stresses

The first busbar support must be situated within the maximum distance (A) from the power terminal of the circuit breaker. This distance is required so that the busbar can withstand the electrodynamic stresses between phases in the event of a short circuit. The table below gives the maximum distance (A) according to the prospective short-circuit current Isc.

Maximum Distance (A) Based on Prospective Short Circuit Current

Maximum Distance A

Short Circuit Current (kA)

Maximum Distance A
mm (in.)

30

350 (13.8)

50

300 (11.8)

65

250 (9.84)

80

150 (5.91)

100

150 (5.91)

Temperature Derating

The current rating of a high-ampere circuit breaker is highly dependent on the actual conditions of installation and connection. Thus it is not possible to give strict values of current rating without performing a temperature rise test in the actual electrical equipment configuration.

Temperature Correction Factors

Maximum Ambient Temperature

°C

70

60

50

40

30

25

20

10

0

-10

-20

-35

-30

°F

158

140

122

104

86

77

68

50

32

14

-4

-13

-22

Current

0.75

0.83

0.92

1

1.07

1.11

1.14

1.21

1.27

1.33

1.39

1.42

1.44

MasterPacT MTZ Minimum Enclosure Sizes

MasterPacT MTZ1

Circuit Breaker

Circuit Breaker Enclosure Dimensions
(H x W x D)

Ventilation Area

Top

Bottom

Front Face

mm

in.

mm2

in.2

mm2

in.2

3P

800 to 1600 A
(N, H, L1)

463.5 x 330.2 x 241.3

18.25 x 13 x 9.5

5,806

9

5,806

9

800 to 1600 A (L)

1581.2 x 584.2 x 374.7

62.25 x 23 x 14.75

10,645

16.5

10,645

16.5

4P

800 to 1600 A
(N, H, L1)

463.5 x 401.3 x 241.3

18.25 x 15.8 x 9.5

5,806

9

5,806

9

800 to 1600 A (L)

1581.2 x 654.2 x 374.7

62.25 x 25.76 x 14.75

10,645

16.5

10,645

16.5

MasterPacT MTZ2 / MTZ3

Circuit Breaker

Enclosure Dimensions
(H x W x D)

Ventilation Area

Top

Bottom

Front Face

mm

in.

mm2

in.2

mm2

in.2

mm2

in.2

3P

≤ 2000 A, UL 1066
(ANSI C37.50)

539.8 x 552.5 x 400

21.25 x 21.75 x 15.75

38,460

59.62

22,980

35.62

≤ 3000 A, UL 489

466.6 x 609.6 x 400

18.37 x 24.00 x 15.75

10,720

16.62

10,720

16.62

3200–4000 A
(MTZ2)

787.4 x 552.5 x 400

31.00 x 21.75 x 15.75

38,460

59.62

60,390

93.6

4000–6000 A, UL 1066
(ANSI C37.50)

838.2 x 828.5 x 400

33.00 x 32.62 x 15.75

128,230

198.75

84,190

130.5

4000–6000 A, UL 489

552.5 x 914.4 x 400

21.75 x 36.00 x 15.75

10,720

16.62

10,720

16.62

4P

≤ 2000 A, UL 1066
(ANSI C37.50)

539.8 x 667.5 x 400

21.25 x 26.28 x 15.75

38,460

59.62

22,980

35.62

≤ 3000 A, UL 489

466.6 x 762.0 x 400

18.37 x 30.00 x 15.75

10,720

16.62

10,720

16.62

3200–4000 A (MTZ2)
UL 1066 (ANSI C37.50)

787.4 x 667.5 x 400

31.00 x 26.28 x 15.75

38,460

59.62

60,390

93.6

4000–6000 A, UL 1066
(ANSI C37.50)

838.2 x 1058.7 x 400

33.00 x 41.68 x 15.75

128,230

198.75

84,190

130.5

4000–6000 A, UL 489

552.5 x 1168.4 x 400

21.75 x 45.00 x 15.75

10,720

16.62

10,720

16.62

MasterPacT MTZ Circuit Breaker Dimensions

Visit the Schneider Electric Download Center to access the following MasterPacT MTZ documents and downloads:

  • MTZ 3D Drawings

  • MTZ 2D Drawings

  • Certificates

  • User Guides

  • Instruction Sheets

MasterPacT MTZ Accessories

Rear Panel Cutout (Drawout Devices)

MTZ1

MTZ2 08 to MTZ2 40

MTZ3 40 to MTZ3 63

Rear View

Rear View

Rear View

Escutcheon

MasterPacT MTZ1

Fixed Device

Drawout Device

MasterPacT MTZ2/MTZ3

Fixed Device

Drawout Device

MasterPacT MTZ External Accessories

Connection of Auxiliary Wiring to Terminal Block

 

One conductor only per connection point.

External Power Supply Module (AD)

ZSI Interface Module

Delay Unit for MN Release

IFE - Ethernet Interface

IFM - Modbus SL (RTU) Interface

IO (Input/Output) Application Module

Com’X 210

Components for Source Ground-Return (SGR) Protection

MGDF Module

Sensor

FDM128

External Neutral Current Sensor

400/1600 A
(MTZ1 06 to MTZ1 16)

400/2000 A
(MTZ2 08 to MTZ2 20)

1000/4000 A
(MTZ2 25 to MTZ2 40)

4000/6300 A
(MTZ3 40 to MTZ3 63)

2000/6300 A
(MTZ2 to MTZ3)
Single Sensor Kit

2000/6300 A
(MTZ2 to MTZ3)
3 Layer Bus

MasterPacT MTZ Clusters

Number of Clusters Per Pole Required for MasterPacT MTZ1 Devices

Device

MTZ1

630 A

6

800 A

6

1000 A

6

1250 A

6

1600 A

6

Number of Clusters Per Pole Required for MasterPacT MTZ2/MTZ3 Devices

Device

MasterPacT MTZ2-3 3P

N / N1

H1

HA

H / H2 / HF

H3

L / L1 / LF / L1F / HB / HC

MTZ2 08

2

4

4

4

6

8

MTZ2 12

2

4

4

8

MTZ2 16

6

6

6

6

6

8

MTZ2 20

8

8

8

8

8

16

MTZ2 25 to 30

16

16

16

MTZ2 32

16

16

16

16

24

MTZ3 40 to 50

24

24

24

24

MTZ3 60

24

24

24

MasterPacT MTZ Enclosure Cutouts

MasterPacT MTZ1 Door Cutout Dimensions

MasterPacT MTZ1 Three-Pole Drawout UL/ANSI Door Cutout

MasterPacT MTZ1 Three-Pole Fixed UL/ANSI Door Cutout Dimensions

MasterPacT MTZ1 Four-Pole Drawout UL/ANSI Door Cutout

MasterPacT MTZ1 Four-Pole Fixed UL/ANSI Door Cutout

MasterPacT MTZ2 Door Cutout Dimensions

MasterPacT MTZ2 Three-Pole and Four-Pole Drawout UL/ANSI Door Cutout

MasterPacT MTZ2 Three-Pole and Four-Pole Fixed UL/ANSI Door Cutout Dimensions

MasterPacT MTZ3 Door Cutout Dimensions

MasterPacT MTZ3 Three-Pole and Four-Pole Drawout UL/ANSI Door Cutout

MasterPacT MTZ3 Three-Pole and Four-Pole Fixed UL/ANSI Door Cutout Dimensions

MasterPacT MTZ2/MTZ3 Mounting

Drawout Cradle Mounting

Fixed Circuit Breaker Mounting

MasterPacT MTZ Shipping Weights

MasterPacT MTZ1 Shipping Weights

Shipping Weights

Circuit Breaker

Circuit Breaker (lb/kg)

Cradle
(lb/kg)

Connector Type and Weight (lb/kg)

Pallet
(lb/kg)

Total Weight
(lb/kg)

Type

Rating (A)

3P

4P

3P

4P

Type

3P

4P

3P

4P

Drawout

800

40/18

52/24

36/16

43/20

FCF

15/7

20/9

10/5

101/46

125/58

1200

RCTH or RCTV

6/3

8/4

10/5

92/42

113/53

Fixed

800

40/18

52/24

FCF

15/7

20/9

10/5

65/30

82/38

1200

RCTH or RCTV

6/3

8/4

10/5

56/26

70/33

1600

40/18

52/24

RCTV

18/8

20/9

10/5

68/31

82/38

MasterPacT MTZ2 Shipping Weights

Shipping Weights

Circuit Breaker

Circuit Breaker (lb/kg)

Cradle
(lb/kg)

Connector Type and Weight
(lb/kg)

Pallet
(lb/kg)

Total Weight
(lb/kg)

Type

Rating (A)

3P

4P

3P

4P

Type

3P

4P

3P

4P

Drawout

800

109/50

142/65

97/44

116/53

FCF

42/19

55/25

17/8

265/121

320/151

1600

FCT

84/38

109/50

17/8

307/140

384/176

2000

RCTH
RCTV

17/8

22/10

17/8

240/110

297/136

2500

127/58

165/75

124/57

149/68

FCT

80/36

104/47

17/8

348/159

435/198

3000

RCTH
RCTV

26/12

34/15

17/8

294/135

365/166

2000
(L1, L1F)

127/58

165/75

124/57

149/68

RCOV (standard)

100/46

130/59

17/8

368/169

461/210

3200
(H1, H2, H3)

RCOV (ArcBlok)

153/69

NA

17/8

421/191

NA

4000 W-Frame
(H1, H2, H3)

RCOV (special)

115/52

145/66

17/8

259/118

327/149

Fixed

800

109/50

142/65

FCF

42/19

55/25

17/8

168/77

204/98

1600

FCT

84/38

109/50

17/8

210/96

368/123

2000

RCTH
RCTV

17/8

22/10

17/8

143/66

181/83

2500

127/58

165/75

FCT

80/36

104/47

17/8

224/102

286/130

3000

RCTH
RCTV

26/12

34/15

17/8

170/78

216/98

2000
(L1, L1F)

127/58

165/75

RCOV (standard

100/46

130/59

17/8

244/112

265/142

3200
(H1, H2, H3)

RCOV (ArcBlok)

153/69

NA

17/8

297/134

NA

4000 W-Frame
(H1, H2, H3)

RCOV (special)

115/52

145/66

17/8

135/61

178/81

MasterPacT MTZ3 Shipping Weights

Shipping Weights

Circuit Breaker

Circuit Breaker (lb/kg)

Cradle
(lb/kg)

Connector Type and Weight (lb/kg)

Pallet
(lb/kg)

Total Weight
(lb/kg)

Type

Rating (A)

3P

4P

3P

4P

Type

3P

4P

3P

4P

Drawout

3200 (L1) 4000

227/103

295/134

278/126

334/152

FCF

84/38

109/50

39/18

628/285

777/354

FCT

168/77

218/99

39/18

712/324

886/403

RCTH
RCTV

52/24

68/31

39/18

596/271

736/335

5000

227/103

295/134

278/126

334/152

FCT

168/77

218/99

39/18

712/324

886/403

RCTH
RCTV

52/24

68/31

39/18

596/271

736/335

6000

227/103

295/134

278/126

334/152

RCTH or RCTV

396/180

528/240

39/18

940/427

1196/544

Fixed

3200 (L1) 4000

227/103

295/134

FCF

84/38

109/50

39/18

350/159

443/202

FCT

168/77

218/99

39/18

634/198

552/251

RCTH
RCTV

52/24

68/31

39/18

318/145

402/183

5000

227/103

295/134

FCT

168/77

218/99

39/18

434/198

552/251

RCTH
RCTV

52/24

68/31

39/18

318/145

402/183

6000

227/103

295/134

RCTH
RCTV

396/180

528/240

39/18

662/301

862/392

MasterPacT MTZ Circuit Breaker Electrical Diagrams

MasterPacT MTZ1 Fixed and Drawout Devices

The diagram is shown with circuits de-energized, all devices open, connected and charged and relays in normal position.

Power*

Control Unit

Indication Contacts

NOTE: It is possible to add a second MX/MX diag&com or a MN/MN diag voltage release. The second MX diag&com voltage release can only be installed after the delivery of the circuit breaker. This is an after-sales adaptation.

Remote Operation*

NOTE: Maximum length of the two wires between A2–A3,/C20C3/C12/C13: 5 m (16 ft.).
For the maximum length of the wiring between the AC/DC power supply and the voltage release terminals A1–A3/C1–C3/C11–C13/D1–D2: see Shunt Close (XF), Shunt Trip (MX), and Undervoltage Release (MN) with Basic Coils.

Terminal Block Marking

Indication Contacts Terminal Bock

 

Control Unit Terminal Block

OF4 / OF3 / OF2 / OF1 : Open/closed indication contacts OF

 

Com :

ULP Communication

Cradle Contacts Terminal Block

 

UC1 :

Z1-Z4 Zone Selective Interlocking
M1 = MDGF module input

CD2 / CD1:

Disconnected position contacts

 

UC2 :

T1, T2 = Neutral External Sensors
M2, M3 = MDGF Module Input

CE3 /CE2 / CE1:

Connected position contacts

 

UC3 :

Voltage Connector (must be connected to the neutral with a 3P circuit breaker)

CT1:

Test position contacts

 
 

UC4 :
or
M2C :

External Voltage Connector (PTE option)

2 Programmable Contacts (external relay) ext. 24 Vdc power supply required is not installed.

 

Remote Operation Terminal Block

 

SDE2:
or
Res: remote reset

Overcurrent Trip Indication Contact

Remote Reset

 

SDE1:

Overcurrent Trip Indication Contact (supplied as standard)

 

MN /MN diag:

Undervoltage Release Standard or Diagnostic

 

MX/MX diag&com:

Shunt Trip Standard or Diagnostic & Communicating

 

2nd MX/MX diag&com:

Shunt Trip Standard or Diagnostic

 

XF/XF diag&com:

Shunt Close Standard or Diagnostic & Communicating

 

PF:

Ready-to-Close Contact

 

MCH:

Spring Charging Motor

NOTE: When communicating MX diag&com or XF diag&com accessories are used, the third wire (C3,A3, C13) must be connected even if the communication module is not installed.

MasterPacT MTZ2/MTZ3 Drawout Devices

The diagram is shown with circuits de-energized, all devices open, connected and charged and relays in normal position.

Power*

Control Unit

Remote Operation

It is possible to add a second MX/MX diag&com or an MN/MN diag coil.

*

Indication Contacts

Cradle Contacts

Control Unit Terminal Block

 

Remote Operation Terminal Block

Com :

ULP communication

 

SDE2:
or
Res:

Overcurrent trip indication contact

Remote Reset

UC1 :

Z1-Z4 Zone Selective Interlocking
M1 = MDGF module input

 
 

UC2 :

T1, T2 = Neutral External Sensors
M2, M3 = MDGF module input ext. 24 Vdc power supply required

 

SDE1:

Overcurrent Trip Indication Contact (Supplied as Standard)

 

MN /MN diag:

Undervoltage Release Standard or Diagnostic

UC3 :

Voltage Connector (must be connected to the neutral with a 3P circuit breaker)

 

MX/MX diag&com:

Shunt Trip Standard or Diagnostic & Communicating

UC4 :
or
M2C :

External Voltage Connector (PTE option)

2 Programmable Contacts (external relay)

 

2nd MX/MX diag&com:

Shunt Trip Standard or Diagnostic

 

XF/XF diag&com:

Shunt Close Standard or Diagnostic & Communicating

 

PF:

Ready-to-Close Contact

     

MCH:

Spring Charging Motor

NOTE: When communicating MX com or XF com accessories are used, the third wire (C3,A3, C13) must be connected even if the communication module is not installed.

Terminal Block Marking

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.