0614CT1701

MasterPacT MTZ Integration in Source-Changeover Systems

Source-Changeover Systems Mechanical Interlocking

Schneider Electric offers source changeover systems based on MasterPacT MTZ devices.

They are made of up to three circuit breakers or switches linked by an electrical interlocking system that may have different configurations. A mechanical interlocking system must be added for additional protection against electrical problems or incorrect manual operations. In addition, a controller can be used for automatically control the source transfer.

For implementing the mechanical interlocking two different possibilities are offered:

  • interlocking with rods

  • interlocking with cables

The following pages present the different solutions for mechanical and electrical interlocking and associated controllers.

Interlocking Two Devices Using Connecting Rods

Interlocking of two MasterPacT MTZ2 or MTZ3 circuit breakers using connecting rods

The two devices must be installed one above the other.

Available only for MasterPacT MTZ2 and MTZ3 devices, all mixed associations between fixed type and drawout type devices are possible.

Installation

This function requires:

  • An adaptation fixture on the right side of each circuit breaker or switch.

  • A set of connecting rods with no-slip adjustments.

  • A mechanical operation counter CDM (required).

The adaptation fixtures, connecting rods, circuit breakers and switches are supplied separately, ready for assembly by the customer.

The maximum vertical distance between the fixing plates is 900 mm (35.4 in.).

Interlocking of Two or Three Devices Using Cables

Interlocking of two MasterPacT circuit breakers using cables

For cable interlocking, the circuit breakers can be installed either one above the other or side-by-side.

All mixed associations between MasterPacT MTZ2 and MTZ3 fixed and drawout type devices are possible.

Interlocking between two MasterPacT MTZ2 devices

This function requires:

  • An adaptation fixture on the right side of each device.

  • A set of cables without slip adjustments.

  • A mechanical operation counter CDM (required).

The maximum distance between the fixing planes (vertical or horizontal) is 2000 mm (78.7 in.).

Interlocking between three MasterPacT MTZ devices.

This function requires:

  • A specific adaptation fixture installed on the right side of each device.

  • Two sets of cables without slip adjustments.

  • A mechanical operation counter CDM (required).

The maximum distance between the fixing planes (vertical or horizontal) is 1000 mm (39.4 in.).

Installation

The adaptation fixtures, sets of cables and circuit breakers or switches are supplied separately, ready for assembly by the customer.

Installation conditions for cable interlocking systems:

  • Cable length: 2.5 m (8.2 ft.)

  • Cable bending radius: greater than 100 mm (3.94 in.)

  • Maximum number of curves: three

NOTE: For cable length higher than 2.5 m (8.2 ft.) please consult Schneider Electric before ordering the circuit breakers for a customized solution.

MasterPacT MTZ Mechanical Interlocking by Cables

All mixed associations between MasterPacT MTZ2 and MTZ3 fixed and drawout type devices are possible.

Cable Interlocking

Vertical

Horizontal

Two devices MTZ2 - MTZ3

Three devices MTZ2 - MTZ3

MasterPacT MTZ1 Circuit Breaker Locking

Catalog Number

Cable-Type Door Interlock


1 complete assembly for MasterPacT MTZ1 fixed devices


LV833920SP


1 complete assembly for MasterPacT MTZ1 drawout devices


LV833921SP

MasterPacT MTZ1 Mechanical Interlocking for Source Changeover Catalog Numbers

 

Catalog Number

Interlocking Using Connecting Rods

Complete assembly with 2 adaptation fixtures + rods

2 MasterPacT MTZ1 fixed devices


LV833203SP

2 MasterPacT MTZ1 drawout devices


LV833204SP

1 set of 2 interlocking rods


LV833210SP

Interlocking Using Cables *

Choose 2 adaptation fixtures (1 for each breaker) + 1 set of cables

1 adaptation fixture for MasterPacT MTZ1 fixed devices

LV833200SP

1 adaptation fixture for MasterPacT MTZ1 drawout devices

LV833201SP

1 set of 2 cables

LV833209SP

Interlocking of 2 devices using connecting rods

Complete assembly with 2 adaptation fixtures + rods

1 set of 2 adaptation fixtures for MasterPacT MTZ2 or MTZ3 fixed or drawout device

LV847930SP

1 set of 2 interlocking rods

LV833210SP

NOTE: Can be used with 1 MTZ2/3 fixed + 1 MTZ2/3 drawout.

Interlocking of 2 Devices Using Cables*

Choose 2 adaptation fixtures (1 for each device) + 1 set of cables

1 adaptation fixture for MasterPacT MTZ2/3 fixed devices

LV847926SP

1 adaptation fixture for MasterPacT MTZ2/3 drawout devices

LV847926SP

1 set of 2 cables of 2.5 m

LV833209SP

Interlocking of 3 Devices Using Cables

Choose 1 interlocking kit (including 3 adaptation fixtures + cables)

3 sources, only 1 device closed, fixed or drawout devices

LV848610SP

2 sources + 1 coupling, fixed or drawout devices

LV848609SP

2 normal + 1 replacement source, fixed or drawout devices

LV848608SP

Door Interlock / 1 Part

Right and left-hand side of cradle (VPECD or VPECG)

LV833772SP

Racking Interlock

Racking interlock (VPOC)

LV833788SP

Spare Parts for Source Changeover Mechanical Interlocking

Catalog Number

Interlocking Using Connecting Rods

Complete assembly with 2 adaptation fixtures + rods

2 MasterPacT MTZ1 fixed devices

NOTE: The installation manual is enclosed.

LV833912SP

2 MasterPacT MTZ1 drawout devices

NOTE: The installation manual is enclosed.

LV833913SP

Interlocking Using Cables *

Choose 2 adaptation fixtures (1 for each device) + 1 set of cables

1 adaptation fixture for MasterPacT MTZ1 fixed devices

LV833200SP

1 adaptation fixture for MasterPacT MTZ1 drawout devices

LV833201SP

1 set of 2 cables

PGL36060

Description

Catalog Number

Door Interlock

Door interlock MTZ1

Right and left-hand side of cradle (VPECD or VPECG)

LV833172SP

Door interlock MTZ2/3

Right and left-hand side of cradle (VPECD or VPECG)

LV847914SP

Cable-type door interlock

1 complete assembly for MasterPacT MTZ2/MTZ3 fixed or drawout device

LV848614SP

Mechanical Interlocking for Source Changeover for MTZ2/3

Interlocking of 2 devices using connecting rods
Choose 1 set of 2 adaptation fixtures (1 for each device) + 1 set of rods

Rod Interlock kit: 1 set of 2 adaptation fixtures for MasterPacT MTZ2 or MTZ3 fixed or drawout device

LV847930SP

1 set of 2 interlocking rods

LV833210SP

Can be used with 1 MTZ2/3 fixed + 1 MTZ2/3 drawout. Note: the installation manual is enclosed. Interlocking of 2 devices using cables [1]

Interlocking of 2 devices using cables [1]
Choose 2 adaptation sets (1 for each device + 1 set of cables)

1 adaptation fixture for MasterPacT MTZ2/3 fixed devices

LV847926SP

Cable mouinting plate: 1 adaptation fixture for MasterPacT MTZ2/3 drawout devices

LV847926SP

Cable interlock: 1 set of 2 cables

LV833209SP

Interlocking of 3 devices using cables
Choose 3 adaptation (including 3 adaptation fixtures + cables)

3 sources, only 1 device closed, fixed or drawout devices

LV848610SP

2 sources + 1 coupling, fixed or drawout devices

LV848609SP

2 normal + 1 replacement source, fixed or drawout devices

LV848608SP

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.