0614CT1701

Cradle Metering CT Kit Catalog Numbers

For use with UL and ANSI rated circuit breakers only. Not available with ArcBlok Technology.

Cradle Metering CT Kit (Set of 3)

Description

Catalog Number

MTZ2 400 A SMCT400
600 A SMCT600
800 A SMCT800
1200 A SMCT1200
1600 A SMCT1600
2000 A SMCT2000
2000 A SMCT2000R
2500 A SMCT2500R
3000 A SMCT3000R
3200 A SMCT3200R
MTZ3 2000 A SMCT2000Y
2500 A SMCT2500Y
3000 A SMCT3000Y
3200 A SMCT3200Y
4000 A SMCT4000Y
5000 A SMCT5000Y
6000 A SMCY6000Y
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.