DOCA0101EN-09

Locking the MasterPacT MTZ3 Safety Shutters

Using Shutter Position Indication and Locking Accessory

Step

Action

1

Pull the shutter indicator arm tabs out of the slot

2

Insert the padlock in the padlock tab and close the padlock.

3

Check that the safety shutters do not open when the actuator is pressed.

Using Shutter Locking Blocks

Step

Action

1

Remove the shutter locking blocks stored in the chassis.

2

Place a shutter locking block on each of the shutter mechanisms. One shutter mechanism per phase:

  • Three shutter locking blocks to lock the 3P device safety shutters

  • Four shutter locking blocks to lock the 4P device safety shutters

3

Insert a padlock in each shutter locking block tab and close the padlock.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.