DOCA0101EN-09

DAE Automatic Spring-Discharge Interlock

Description

The DAE automatic spring-discharge interlock releases the closing spring energy when a drawout MasterPacT MTZ2/MTZ3 device is moved from the disconnected position to the withdrawn position.

The DAE interlock is an optional interlock mounted inside the device. It is factory-installed. To install it on site, contact your Schneider Electric Services representative.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.