DOCA0101EN-09

Control Modes

@writer (10/2020): this topic is present in user guides: MTZ1 (DOCA0100EN) + MTZ2/3 (DOCA0101EN) + MicroLogic X (DOCA0102EN).

Presentation

The circuit breaker control mode is a MicroLogic X setting which defines the means to control the opening and closing functions of the circuit breaker.

Two control modes are available: Manual and Auto.

Manual control mode only accepts orders made using one of the following:

  • The mechanical buttons on the front of the circuit breaker.

  • The external pushbutton connected to the MN/MX/XF voltage releases.

  • The BPFE electrical closing pushbutton.

Auto control mode has two settings: Local or Remote. All orders accepted in Manual control mode are accepted in Auto control mode, as well as orders from local or remote communication as follows:

  • Auto Local: the operator needs to be close to the circuit breaker to establish communication and only orders sent from a local source through communication are accepted:

    • EcoStruxure Power Commission software through USB connection

    • EcoStruxure Power Device app with MasterPacT Operation Assistant Digital Module through Bluetooth Low Energy or USB OTG connection

  • Auto Remote: the operator does not need to be next to the circuit breaker to establish communication and orders are accepted only when sent from a remote source through the communication network.

NOTE: EcoStruxure Power Commission software connected through the communication network can be used to send control orders to the circuit breaker.

The control mode factory setting is Auto Remote.

NOTE: The switch-disconnector control mode corresponds to the Manual control mode of circuit breakers. To operate a switch-disconnector through communication, it is possible to use an IO module. Refer to Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide in Related Documents at the beginning of this guide.

Operation According to Control Mode Configured

The following table summarizes the opening and closing operations available, depending on the control mode configured:

Control mode

Type of order and delivery method

Mechanical

Electrical

Through communication

Pushbutton

BPFE

Point to point (voltage release)

IO module

FDM121 display

EcoStruxure Power Commission software (1)

EcoStruxure Power Device app + MasterPacT Operation Assistant Digital Module(2)

Communication network

FDM128 display

IFE/EIFE Weblogs

Manual

Auto: Local

(3)

Auto: Remote

(3)

(1) Through USB

(2) Through Bluetooth Low Energy or USB OTG connection

(3) According to IO input mode setting

Operation in Manual Control Mode

A MicroLogic X control unit

B ULP port module

C EIFE embedded Ethernet interface

D Circuit breaker mechanism

Opening and closing operations available in Manual control mode:

  • 0: mechanical opening pushbutton

  • 1: mechanical closing pushbutton

  • BPFE: electrical closing pushbutton

  • External pushbuttons wired by customer, and connected to:

    • XF: standard or communicating and diagnostic closing voltage release

    • MX: standard or communicating and diagnostic opening voltage release

    • MN: standard or diagnostic undervoltage release

Operation in Auto: Local Mode

A MicroLogic X control unit

B ULP port module

C EIFE embedded Ethernet interface

D Circuit breaker mechanism

E IO input/output application module

Opening and closing operations available in Auto: Local mode:

  • 0: mechanical opening pushbutton

  • 1: mechanical closing pushbutton

  • BPFE: electrical closing pushbutton

  • External pushbuttons wired by customer, and connected to:

    • XF: communicating and diagnostic closing voltage release

    • MX: communicating and diagnostic opening voltage release

    • MN: standard or diagnostic undervoltage release

  • IO: with the Breaker Operation predefined application of the IO module set to local control mode

  • EcoStruxure Power Commission software: command sent through USB connection

  • EcoStruxure Power Device app with MasterPacT Operation Assistant Digital Module:

    • Through Bluetooth Low Energy wireless communication

    • Through USB OTG connection

Operation in Auto: Remote Mode

A MicroLogic X control unit

B ULP port module

C EIFE embedded Ethernet interface

D Circuit breaker mechanism

E IO input/output application module

Opening and closing operations available in Auto: Remote mode:

  • 0: mechanical opening pushbutton

  • 1: mechanical closing pushbutton

  • BPFE: electrical closing pushbutton

  • External pushbuttons wired by customer, and connected to:

    • XF: communicating and diagnostic closing voltage release

    • MX: communicating and diagnostic opening voltage release

    • MN: standard or diagnostic undervoltage release

  • IO: with the Breaker Operation predefined application of the IO module set to remote control mode

  • Communication: remote command through IFE, EIFE, or IFM interface.

Setting the Control Mode

The Auto or Manual control mode can be set as follows:

  • On the MicroLogic X display screen, at Home > Configuration > Communication > Control Mode > Mode.

  • With the EcoStruxure Power Device app through Bluetooth Low Energy or USB OTG connection.

The Local or Remote mode can be set as follows:

  • When the IO module is used with the Breaker Operation predefined application, the local or remote mode is defined only by the control mode selector switch wired on the digital input I1 of the IO module.

  • When the IO module is not used with the Breaker Operation predefined application, the local or remote mode can be set as follows:

    • With EcoStruxure Power Commission software through USB connection.

    • With the EcoStruxure Power Device app through Bluetooth Low Energy or USB OTG connection.

    • With the FDM121 display connected to the MicroLogic X control unit through the ULP system.

NOTE:
  • The Local or Remote mode cannot be set on the MicroLogic X display screen.

  • When Auto control mode is set, the control mode is Auto Local or Auto Remote, depending on the last setting.

Displaying the Control Mode

The control mode (Manual, Auto Local, or Auto Remote) is displayed as follows:

  • On the MicroLogic X display screen, at Home > Configuration > Communication > Control Mode > Mode

  • With EcoStruxure Power Commission software through USB connection

  • With the EcoStruxure Power Device app through Bluetooth Low Energy or USB OTG connection

  • On the IFE/EIFE webpages

  • By a remote controller using the communication network.

Predefined Events

Changing the control mode settings generates the following events:

Code

Event

History

Severity

0x1002 (4098)

Manual mode enabled

Operation

Low

0x1004 (4100)

Local mode enabled

Operation

Low

0x0D0D (3341)

Config. error IO and CU - Local/Remote mode

Configuration

Medium

Recommended Actions

Code

Event

Recommended actions

0x0D0D (3341)

Config. error IO and CU - Local/Remote mode

Correct the configuration error with EcoStruxure Power Commission:

  • If you want the L/R mode to be controlled by the IO module, connect an IO module with L/R mode assignment.

  • If you do not want the L/R mode to be controlled by the IO module, connect an IO module without L/R mode assignment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.