DOCA0101EN-09

Inspection and MicroLogic X Settings

@writer: This topic is present in MTZ1 and MTZ2-3 (Commissioning). Any changes made will be made in all these guides.

Visual Inspection

Step

Action

1

Record the equipment identification, including substation name, switchboard name, MasterPacT MTZ device type, MicroLogic X model type and serial number, MicroLogic X type, and protection settings.

2

Check that the device is undamaged, correctly mounted, and securely fastened in the switchboard.

3

Check the 3-phase clearance at terminal blocks.

4

Check that there is no debris remaining at the back of the device housing/enclosure.

5

Check that the ground terminals of the device are securely connected with the correct grounding cables.

6

Check that all external surfaces are undamaged.

7

Rectify any non-conformities, if possible. All equipment non-conformities must be referred to asset management.

Condition of Connections and Auxiliaries

Check device mounting in the switchboard and the tightness of all connections (main connection and auxiliary wiring).

Check that all auxiliaries and accessories are correctly installed:

  • Electrical auxiliaries

  • Terminal blocks

  • Connections of auxiliary circuits

Check Firmware Compatibility

By using the latest version of EcoStruxure Power Commission software, check that the firmware of the MicroLogic X control unit and ULP modules in the intelligent modular unit (IMU) are up-to-date, compatible with each other, and are compatible with the Digital Modules that are installed. The ULP modules are EIFE, IFE, or IFM communication interfaces, IO module, and FDM121 display.

Step

Action

1

Connect a PC running EcoStruxure Power Commission software by using a cable connected to the mini USB port on the front face of the MicroLogic X control unit.

2

Establish a connection. EcoStruxure Power Commission software reads the parameters of the control unit.

3

On EcoStruxure Power Commission, use the Overall System firmware status/compatibility matrix to display:

  • The installed firmware version of the IMU devices (MicroLogic X control unit and ULP modules).

  • The latest firmware version of the devices that are available on the Schneider Electric System Updates Internet site.

  • The recommended actions to get a compatible system.

For more information, refer to EcoStruxure Power Commission Online Help.

NOTE: The FDM121 display firmware version must be 004.000.009 or greater to be compatible with MicroLogic X control units. Earlier firmware versions need to be updated, refer to Troubleshooting.

4

Follow the recommended actions to get a compatible system.

MicroLogic X Settings

NOTICE
RISK OF UNINTENDED OPERATION
  • The device must only be configured and set by qualified personnel, using the results of the installation protection system study.
  • During commissioning of the installation and following any modification, check that the MicroLogic B/BP configuration and protection function settings are consistent with the results of this study.
  • MicroLogic B/BP protection functions are set by default to the minimum value, except for the long time protection function which is set to the maximum value, by default.
Failure to follow these instructions can result in equipment damage.

Check the settings with EcoStruxure Power Commission software connected to the MicroLogic X control unit.

Step

Action

1

Connect a PC running EcoStruxure Power Commission software by using a cable connected to the mini USB port on the front face of the MicroLogic X control unit.

2

Establish a connection. EcoStruxure Power Commission software reads the parameters of the control unit.

3

Check that the settings read in the control unit match the requirements of the application. If necessary, correct the settings with EcoStruxure Power Commission software:

  • The protection settings must be defined according to the installation protection system study.

  • Other settings must be defined according to the application.

4

Check that the date and time are set. If necessary, set them on the MicroLogic X display screen at Home > Configuration > General > Date & time.

5

Complete the project and device data.

6

Generate the project report with EcoStruxure Power Commission software, and save or print the project report as needed.

NOTE: The protection functions available depend on the type of MicroLogic X control unit and its associated optional Digital Modules.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.