DOCA0101EN-09

Introduction to Troubleshooting

@writer: (confirmed 12/11/24) topic shared in Masterpact MTZ1 User Guide (DOCA0100), Masterpact MTZ2/3 User Guide (DOCA0101), and in the appendix in Masterpact MTZ End-user and Manufacturer Maintenance Procedures (DOCA0103 and DOCA0104). Any changes made will be made in all these guides.

Presentation

This part contains information for troubleshooting problems in a working system. It assumes that the system is correctly installed and that all the commissioning tests have been completed successfully. The troubleshooting operations are described under the following headings:

Layer Model

When troubleshooting the device, it is useful to consider a layer model. There are four layers:

  • Communication network

  • Direct connection

  • Electrical

  • Mechanical

The following diagram shows the layers in the device:

Communication network

Direct communication

Electrical

Mechanical

If the troubleshooting actions for a layer are not successful, go to the next layer until you reach the Mechanical layer. If you cannot solve the problem after troubleshooting the Mechanical layer, contact your Schneider Electric Services representative.

Troubleshooting with Assistance

Assistance for troubleshooting is provided by the MasterPacT Operation Assistant Digital Module.

The MasterPacT Operation Assistant Digital Module helps to close a circuit breaker after a trip or an opening.

The following features are available:

  • Ready-to-close status

  • Reset (if applicable)

  • Spring charging (if applicable)

  • Diagnostics on related reclosing information, for example, no power supply to MX opening voltage release, MN undervoltage release, or MCH gear motor

For more information about downloading Digital Modules, refer to DOCA0102•• MasterPacT MTZ - MicroLogic X Control Unit - User Guide in Related Documents at the beginning of this guide.

Maintenance of the Device

Schneider Electric recommends a preventive maintenance program to ensure that devices retain the operating and technical characteristics specified in the catalogs during their service life. Maintenance must be carried out by trained and qualified personnel.

For information about the preventive maintenance program and maintenance procedures, refer to DOCA0099•• MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide in Related Documents at the beginning of this guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.