DOCA0101EN-09

Mismatch Protection

Description

Mismatch protection allows the installation of a MasterPacT MTZ2/MTZ3 device only in a chassis with compatible characteristics.

Mismatch protection offers 35 different combinations that can be selected so that a device can only be mounted on a chassis with the matching combination.

Accessory

The use of mismatch protection is optional. One mismatch protection accessory is required for each device.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35465.

Pin Location of Mismatch Protection

The following illustration shows the pin location on the chassis and device, respectively.

The pin combination selected on the chassis must correspond to the pin combination selected on the device (see following table). For example, the combination ABCD on the chassis corresponds to the combination 567 on the device.

Pins on the chassis are labeled A, B, C, D, E, F, G.

Pins on the device are labeled 1, 2, 3, 4, 5, 6, 7.

Recommended Pin Combinations

The following are the recommended pin combinations:

Pins on chassis

Pins on device

Pins on chassis

Pins on device

ABCD

567

BCDE

167

ABCE

467

BCDF

157

ABCF

457

BCDG

156

ABCG

456

BCEF

147

ABDE

367

BCEG

146

ABDF

357

BCFG

145

ABDG

356

BDEF

137

ABEF

347

BDEG

136

ABEG

346

BDFG

135

ABFG

345

BEFG

134

ACDE

267

CDEF

127

ACDF

257

CDEG

126

ACDG

256

CDFG

125

ACEF

247

CEFG

124

ACEG

246

DEFG

123

ACFG

245

   

ADEF

237

   

ADEG

236

   

ADFG

235

   

AEFG

234

   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.