DOCA0101EN-09

Device Interlocking Actions

About Interlocking Actions

An interlocking action is an automatic locking operation provided by interlocking accessories added to the MasterPacT MTZ2/MTZ3 device or chassis.

A number of optional interlocking accessories are available for the MasterPacT MTZ2/MTZ3 device and chassis. For a complete listing of available interlocks, refer to LVPED216026EN MasterPacT MTZ with MicroLogic X Control Unit - Catalog.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.