DOCA0101EN-09

IPA Cable-type Door Interlock

Description

When the cable-type door interlock is installed, the door cannot be opened when the device is closed and the device cannot be closed when the door is open.

The cable-type door interlock comprises a plate, a lock and a cable. It is mounted on the right-hand side of the device.

When the interlock is installed, the mechanical interlock for transfer switches cannot be implemented.

Accessory

The IPA cable-type door interlock is an optional accessory.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35495.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.