DOCA0101EN-09

MasterPacT MTZ2/MTZ3 Range

Description

The MasterPacT MTZ2/MTZ3 range of circuit breakers and switch-disconnectors offers current ratings from 800 A to 6,300 A, for AC power systems up to 1,150 Vac.

The MasterPacT MTZ2/MTZ3 range is available in the following frame sizes:

  • MasterPacT MTZ2 for current ratings from 800 A to 4,000 A

  • MasterPacT MTZ3 for current ratings from 4,000 A to 6,300 A

Each frame size is available in the following power systems:

  • 3-pole (3P)

  • 4-pole (4P)

Devices are available in the following installation types:

  • Fixed-mounted devices

  • Drawout devices

Convention

In this guide, the term MasterPacT MTZ device covers circuit breakers and switch-disconnectors.

Circuit Breakers

The following performance levels are available:

  • N1: standard short-circuit level (42 kA) with total selectivity

  • H1: high short-circuit level (66 kA) with total selectivity

  • H2: very high short-circuit level (100 kA) with very high selectivity (85 kA)

  • H2V: very high short-circuit level (100 kA) with very high selectivity (100 kA) (Rated operational voltage Ue limited to 440 Vac)

  • H3: extremely high short-circuit level (150 kA) with high selectivity (66 kA)

  • L1: extremely high short-circuit level (150 kA) with strong current limitation and significant selectivity (30 kA)

NOTE: The values above correspond to a 440 Vac network, for higher voltage levels the values can be different. Refer to LVPED216026EN MasterPacT MTZ with MicroLogic X Control Unit - Catalog.

Circuit breakers are fitted with a MicroLogic X control unit.

For full information about available circuit breaker models, frame sizes, interrupting ratings, sensor ratings, and control units, refer to LVPED216026EN MasterPacT MTZ with MicroLogic X Control Unit - Catalog.

Switch-Disconnectors

The following performance levels are available:

  • NA: Icw = 42 kA/1s

  • HA: Icw = 66 kA/1s

  • HF: Icw = 85 kA/1s

  • HH: Icw = 100 kA/1s

For information about available switch-disconnector models and frame sizes, refer to LVPED216026EN MasterPacT MTZ with MicroLogic X Control Unit - Catalog.

Neutral Position on 4P Devices

On 4P circuit breakers:

  • For MasterPacT MTZ2 N1, H3, L1, H10, the neutral position is on the left side as standard.

  • For MasterPacT MTZ2 H1, H2, and H2V, the neutral position is on the left side as standard. A version with neutral position on the right side is available when ordering.

  • For MasterPacT MTZ3 H1, H2, the neutral position is on the left side as standard. A version with neutral position on the right side is available when ordering.

On 4P switch-disconnectors:

  • For MasterPacT MTZ2 NA, HA, HF, the neutral position can be switched from the left side to the right side using the label provided.

  • For MasterPacT MTZ2 HH, the neutral position is on the left side as standard. A version with neutral position on the right side is available when ordering.

  • For MasterPacT MTZ3 HA, the neutral position is on the left side as standard.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.