DOCA0101EN-09

Final Checks and Reporting

This topic is present in MTZ1 and MTZ2-3 (Commissioning). Any changes made will be made in all these guides.

Final Checks

After completing the commissioning tests, check the following:

Step

Action

1

Check that connections are made with the correct tightening torque, that there are no tools or objects inside the equipment, and that all devices, doors, and protective covers are in position.

2

Check that the device is off (open position) and the closing spring is charged.

Project Report Generated by EcoStruxure Power Commission Software

EcoStruxure Power Commission software generates a project report with a list of the circuit breakers for that project. For each MasterPacT MTZ circuit breaker it provides the following information:

  • The circuit breaker identification data

  • The MicroLogic X identification data, including the list of Digital Modules installed

  • The list of accessories including internal accessories (for example, M2C programmable contacts), and external modules (for example, IO module)

  • The protection settings for the MicroLogic X control unit

  • The alarm settings

  • The IFE, EIFE, or IFM communication interface settings

@writer (20/06/2016): FYI, “tests results are not part of the project report” (sesa59748, 7/06/2016)

Communication Test Report Generated by EcoStruxure Power Commission Software

EcoStruxure Power Commission software performs a communication test and generates a report of the test. For each communicating device it provides the following information:

  • The name and type of the device

  • The type of communication

  • The address of the device

  • The status of the connection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.