DOCA0101EN-09

VPEC Door Interlock

Description

With the door interlock:

  • The equipment door is locked and cannot be opened when the drawout device is in connected or test position.

  • The equipment door can be opened when the drawout device is in disconnected position.

  • The equipment door can be closed with the drawout device in any position.

Accessory

The VPEC door interlock accessory is an optional accessory that is mounted on the left side or on the right side of the chassis. One door interlock is necessary for each chassis.

For information on the accessory installation, consult the instruction sheet on the Schneider Electric website: NVE35493.

Locking the Equipment Door

Step

Action

1

Close the equipment door.

2

Put the device into the test or connected position.

3

Check that the equipment door is locked.

Unlocking the Equipment Door

Step

Action

1

Put the device into the disconnected position.

2

Check that the equipment door is unlocked.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.