Multi Carrier Systems and Stepper Drives

Motion Control

Lexium MC12 Multi Carrier

Image Callout

The Lexium MC 12 Multi Carrier System is an innovative transportation system for moving, positioning or grouping objects in machines for discrete processes. It consists of long stator motors on which multiple carrier units can be moved independently from each other. This creates new freedom for designing faster and more flexible machines with less footprint. Typical fields of applications are, for example, packaging and filling processes or assembly applications.

Links to Websites and Downloads:

Lexium MC12 Multi Carrier on www.se.com/us

Lexium MC12 Catalog Document Number DIA7ED2210701EN

Lexium SD3 and Motors

Lexium SD3 Stepper Drives and Motors

3-phase stepper drives and stepper motors for motion control.

The Lexium SD3 with its excellent constant velocity characteristics is ideal for applications such as scanning. High torque is available even at low speeds. Therefore, the stepper motor is particularly suitable for short-distance positioning, such as labelling. It also provides a high holding torque, yet another advantage that makes it an optimum solution in applications such pick and place, etc.


Links to Websites and Downloads:

SD3 Stepper Drives and Motors on www.se.com/us

Feedback