DOCA0131EN-03

Firmware Update Policy

Firmware update is recommended to benefit from the latest features and potential bug fixes. Update the firmware to the latest version when the latest features and bug fixes are required for your application. Use the firmware release notes to confirm if an update to the latest version of the firmware is relevant for your application. The latest firmware and release notes can be found together by searching for "TeSys T Firmware" at www.se.com.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?