PROFIBUS DP Profile
Introduction
The LTMR controller is compliant with the Motor Management Starter (MMS) device class according to the Low Voltage Switchgear (LSVG) PROFIBUS DP profile.
The cyclic data of these devices uses edge triggered signals.
Operational States
|
Sequence |
Description |
|---|---|
|
0 |
Device switched OFF (no current, no internally stored switch-ON command) |
|
1 |
REVERSE/FORWARD command activated |
|
1.1 |
- actual or internally stored switch-ON command activated |
|
1.2 |
- after a delay time, current will be measured |
|
1.3 |
- a measured current in addition to the actual or internally stored switch-ON command (RUN REVERSE/FORWARD) impacts the confirmation signal RUN FORWARD/REVERSE (will be set to high) |
|
2 |
OFF command activated |
|
2.1 |
- the confirmation signal RUN FORWARD/REVERSE will be cleared to low |
|
2.2 |
- after a motor stop, no current will be measured |
|
2.3 |
- no current and no (internally) stored switch-ON command impacts the OFF signal |
Type and Size of Cyclic Data
The size and type of the cyclic data exchanged depend on whether or not modules with PKW are selected during configuration.
The table below indicates the size and type of cyclic data for each module.
|
Module |
Inputs |
Outputs |
|
|---|---|---|---|
|
Without |
MMC R |
10 status bytes (= 4 status words) |
6 command bytes (= 3 command words) |
|
MMC R EV40 |
|||
|
MMC L |
|||
|
MMC L EV40 |
|||
|
With |
MMC R PKW |
10 status bytes (= 4 status words) + 8 PKW in bytes (= 4 PKW in words) |
6 command bytes (= 3 command words) + 8 PKW out bytes (= 4 PKW out words) |
|
MMC R PKW EV40 |
|||
|
MMC L PKW |
|||
|
MMC L PKW EV40 |
The 8 status bytes and 6 command bytes are common to all modules.
Modules with PKW exchange 8 additional bytes dedicated to PKW function PKW: Encapsulated Acyclic Accesses in DP V0 .
Cyclic Data Format
Depending on the PLC platform used, cyclic data bytes are seen and organized differently.
To facilitate LTMR setup, cyclic data are described according to the following formats:
-
Byte format (used by Siemens PLCs for example)
-
Word little endian format (used by Premium PLCs for example)
-
Word big endian format (used by Siemens PLCs for example)