DOCA0131EN-03

PROFIBUS DP Protocol Principle and Main Features

Overview

PROFIBUS DP is an open industrial standard for integrated communication. It is a serial fieldbus, which provides a decentralized connection between sensors, actuators and I/O modules produced by various manufacturers, and connects them to the superset control level.

PROFIBUS DP (Distributed Periphery - Primary/Secondary Network) is a PROFIBUS communication profile which is optimized for performance. It is optimized for speed, efficiency and inexpensive hook-up cost and is designed especially for communication between automation systems and distributed peripheral equipment.

The PROFIBUS DP network supports multiple primary systems with several secondaries.

The PROFIBUS DP protocol is a primary-secondary protocol:

PROFIBUS DP Features

The following table contains specifications of the PROFIBUS DP:

Standard

EN 501 70

DIN 19245

Transmission Equipment (Physical Profile)

EIA RS-485

Transfer Procedure

Half-duplex

Bus Topology

Linear bus with active bus termination

Bus Cable Type

Shielded, twisted-pair conductors

Connector

SUB-D 9-pin

Open style

Number of Nodes on the Bus

Maximum of 32 with no repeaters

Maximum of 125 with three repeaters in four segments

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.