PROFIBUS DP Configuration via the SyCon Configuration Tool
Introduction
With SyCon software, you can configure the PROFIBUS DP network and generate an ASCII file to import into the PLC configuration into Unity Pro (or PL7 or Concept).
Network conditions
The network conditions for the example are
-
Protocol: PROFIBUS DP
-
Address: 4
-
Baud rate: 3 Mb/s
Configuration of a TeSys T System
Example of a network configuration:
|
Step |
Action |
|---|---|
|
1 |
Import your GSD file with . |
|
2 |
Select the path where GS*-files have been unzipped, and click OK. |
|
3 |
Insert a primary (master): |
|
4 |
Select the network speed:
The PROFIBUS DP secondaries (slaves) adapt automatically their baud rate to the primary (master) baud rate. |
|
5 |
In the window, select a primary
(master) (for example, Press the button and confirm with . |
|
6 |
Insert a secondary (slave): |
|
7 |
In the window, select |
|
8 |
Select
Note: Refer to Modules as Presented in the GS*-File. Go on with steps 9 to 12 if a Remote (R) configuration mode has been selected. |
|
9 |
Click the button to open the window. |
|
10 |
Click the button to open the corresponding window and set the parameter values. |
|
11 |
Click OK. |
|
12 |
Click the button of each open dialog window to confirm the selected parameter values. |
Save and Export the Network Configuration
Save and export the configuration for importation into the PLC configuration (PL7, Concept or Unity Pro).
|
Step |
Action |
|---|---|
|
1 |
Select to open the window. |
|
2 |
Choose the and a and click (extension .pb). |
|
3 |
Select to export the configuration as an ASCII file (extension .cnf). |
|
4 |
Import the PROFIBUS DP configuration into the PLC configuration (PL7, Concept or Unity Pro). |