DOCA0131EN-03

User Map Variables

User Map Variables

User Map variables are described in the following table:

User Map Variable Groups

Registers

User Map addresses

800 to 899

User Map values

900 to 999

Register

Variable Type

Read/Write Variables

Note

800-898

Word[99]

User map addresses setting

 

899

 

(Reserved)

 

Register

Variable Type

Read/Write Variables

Note

900-998

Word[99]

User map values

 

999

 

(Reserved)

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?