Modules as Presented in the GS*-File
Overview
The TeSys T system is presented as a "modular device" on PROFIBUS DP.
You must select one of the modules described in the following sections with/without PKW during configuration.
The TeSys T system is described by a GS*-file. This file is used by any PROFIBUS DP configuration tool to get information about the device.
GS*-Files
The file for the PROFIBUS DP LTMR is called CCCCCC.GS*. The asterisk (*) is replaced by E for English, F for French, G for German, and so on (D for Default).
-
For the GSx files 2.01, CCCCCC stands for SE210B48.GSx.
-
For the GSx files 2.02, CCCCCC stands for SE220B48.GSx.
The GS*-files and icons associated with the LTMR can be downloaded from www.se.com website (). GS*-files and icons are grouped in a single compressed Zip file that you must unzip to a single directory on your hard disk drive.
DANGER |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Do not modify the GS*-file in
any way.
Modifying the GS*-file
can cause unpredictable behavior of the devices.
Failure to follow these instructions will result in death or serious injury.
|
Modules Without PKW
Short and long description of modules without PKW:
|
Short Description as Shown in the General Station Description (GSD) |
Long Description |
|---|---|
|
MMC R |
Motor Management Controller, remote configuration mode |
|
MMC R EV40 |
Motor Management Controller, LTMEV40, remote configuration mode |
|
MMC L |
Motor Management Controller, local configuration mode |
|
MMC L EV40 |
Motor Management Controller, LTMEV40, local configuration mode |
In local configuration mode, the parameter Config via Network Port Enable must be disabled. This mode preserves the local configuration made via the HMI port.
In remote configuration mode, the parameter Config via Network Port Enable must be enabled. This mode enables the configuration of the MMC through the network.
Modules without PKW exchange cyclically 10 input bytes (5 input words) and 6 output bytes (3 output words).
Modules with PKW
Short and long description of modules with PKW:
|
Short Description as Shown in the GSD |
Long Description |
|---|---|
|
MMC R PKW |
Motor Management Controller, remote configuration mode with PKW |
|
MMC R PKW EV40 |
Motor Management Controller, LTMEV40, remote configuration mode with PKW |
|
MMC L PKW |
Motor Management Controller, local configuration mode with PKW |
|
MMC L PKW EV40 |
Motor Management Controller, LTMEV40, local configuration mode with PKW |
The PKW feature is implemented to allow acyclic read or write access to any register using cyclic data. It is useful with Primary DP V0.
Modules with PKW exchange cyclically 18 input bytes (9 input words) and 14 output bytes (7 output words).
DANGER