Command Variables
Command Variables
Command variables are described in the following table:
|
Register |
Variable Type |
Read/Write Variables |
|
|---|---|---|---|
|
700 |
Word |
Register available to remotely write commands that can be processed in a specific custom logic |
|
|
701-703 |
(Reserved) |
||
|
704 |
Word |
Control register 1 |
|
|
bit 0 Motor run forward command * |
|||
|
bit 1 Motor run reverse command * |
|||
|
bit 2 (Reserved) |
|||
|
bit 3 Trip reset command |
|||
|
bit 4 (Reserved) |
|||
|
bit 5 Self test command |
|||
|
bit 6 Motor low speed command |
|||
|
bits 7-15 (Reserved) |
|||
|
705 |
Word |
Control register 2 |
|
|
bit 0 clear all command Clear all parameters, except:
|
|||
|
bit 1 clear statistics command |
|||
|
bit 2 clear thermal capacity level command |
|||
|
bit 3 clear controller settings command |
|||
|
bit 4 clear network port settings command |
|||
|
bits 5-15 (Reserved) |
|||
|
706-709 |
(Reserved) |
||
|
710-799 |
(Forbidden) |