PKW: Encapsulated Acyclic Accesses in DP V0
Overview
Some PROFIBUS DP primaries (masters) do not provide DP V1 services. The PKW feature is implemented to allow acyclic read or write access in DP V0.
This feature is enabled in the PROFIBUS DP configuration tool by selecting the appropriate module. For each module, a second entry with PKW exists.
The PKW data is added to the cyclic data.
Read/Write Registers
With the PKW data, you can read or write any register. The 8 bytes are interpreted as a request telegram or a response telegram encapsulated in IN data and OUT data.
PKW OUT Data
PKW OUT Data request (PROFIBUS DP Master → LTMR) are mapped in modules supporting PKW.
To access a register, you must select 1 of the following function codes:
-
R_REG_16 = 0x25 to read 1 register
-
R_REG_32 = 0x26 to read 2 registers
-
W_REG_16 = 0x2A to write 1 register
-
W_REG_32 = 0x2B to write 2 registers.
Register numbers are given in Register Map (Organization of Communication Variables).
|
Word 1 |
Word 2 |
Word 3 |
Word 4 |
||
|---|---|---|---|---|---|
|
Register address |
Toggle bit (bit 15) |
Function bits (bits 8 to 14) |
Not used (bits 0 to 7) |
Data to write |
|
|
Register number |
0/1 |
R_REG_16 Code 0x25 |
0x00 |
_ |
_ |
|
R_REG_32 Code 0x26 |
_ |
_ |
|||
|
W_REG_16 Code 0x2A |
Data to write in register |
_ |
|||
|
W_REG_32 Code 0x2B |
Data to write in register 1 |
Data to write in register 2 |
|||
Depending on the PLC platform used, refer to the tables describing PKW OUT in Little and Big endian formats in the section Cyclic Data Description to know the positioning of each field inside each word.
Any changes in the function field will trigger the handling of the request (except if Function code = 0x00).
The toggle bit must change at each consecutive request. This mechanism allows the request initiator to detect that a response is ready by polling the toggle bit in response. When this bit in the OUT data becomes equal to the response emitted toggle bit in the IN data, then the response is ready.
PKW IN Data
PKW IN Data Response (LTMR → PROFIBUS DP Master) is mapped in modules supporting PKW. The LTMR echoes the same register address and function code or eventually a detected error code:
|
Word 1 |
Word 2 |
Word 3 |
Word 4 |
||
|---|---|---|---|---|---|
|
Register address |
Toggle bit (bit 15) |
Function bits (bits 8 to 14) |
Not used (bits 0 to 7) |
Data to write |
|
|
Same register number as in request |
Same as request |
DETECTED ERROR Code 0x4E |
0x00 |
Detected error code |
|
|
R_REG_16 Code 0x25 |
Data read in register |
_ |
|||
|
R_REG_32 Code 0x26 |
Data read in register 1 |
Data read in register 2 |
|||
|
W_REG_16 Code 0x2A |
_ |
_ |
|||
|
W_REG_32 Code 0x2B |
_ |
_ |
|||
Depending on the PLC platform used, refer to the tables describing PKW IN in Little and Big endian formats in the section Cyclic Data Description to know the positioning of each field inside each word.
If the initiator tries to write a TeSys T object or register to an unauthorized value, or tries to access an inaccessible register, a detected error code is answered (Function code = toggle bit + 0x4E). The exact detected error code can be found in words 3 and 4. The request is not accepted and the object or register remains at the old value.
If you want to re-trigger exactly the same command, you must:
-
Reset the Function code to 0x00,
-
Wait for the response frame with the function code equal to 0x00, then
-
Set it again to its previous value.
This is useful for a limited primary (master) like an HMI.
Another way of re-triggering exactly the same command is to:
-
Invert the toggle bit in the function code byte.
The response is valid when the toggle bit of the response is equal to the toggle bit written in the answer (this is a more efficient method, but it requires higher programming capabilities).
PKW Detected Error Codes
Detected Write Errors
|
Detected Error Code |
Detected Error Name |
Explanation |
|---|---|---|
|
1 |
FGP_ERR_REQ_STACK_FULL |
external request: sends back a detected error frame |
|
3 |
FGP_ERR_REGISTER_NOT_FOUND |
register not managed (or the request needs super user access rights) |
|
4 |
FGP_ERR_ANSWER_DELAYED |
external request: answer postponed |
|
7 |
FGP_ERR_NOT_ALL_REGISTER_FOUND |
one or both registers cannot be found |
|
8 |
FGP_ERR_READ_ONLY |
register not authorized to be written |
|
10 |
FGP_ERR_VAL_1WORD_TOOHIGH |
written value not in the range of the register (word value is too high) |
|
11 |
FGP_ERR_VAL_1WORD_TOOLOW |
written value not in the range of the register (word value is too low) |
|
12 |
FGP_ERR_VAL_2BYTES_INF_TOOHIGH |
written value not in the range of the register (MSB value is too high) |
|
13 |
FGP_ERR_VAL_2BYTES_INF_TOOLOW |
written value not in the range of the register (MSB value is too low) |
|
16 |
FGP_ERR_VAL_INVALID |
written value not a valid value |
|
20 |
FGP_ERR_BAD_ANSWER |
external request: sends back a detected error frame |
Detected Read Errors
|
Detected Error Code |
Detected Error Name |
Explanation |
|---|---|---|
|
1 |
FGP_ERR_REQ_STACK_FULL |
external request: sends back a detected error frame |
|
3 |
FGP_ERR_REGISTER_NOT_FOUND |
register not managed (or the request needs super user access rights) |
|
4 |
FGP_ERR_ANSWER_DELAYED |
external request: answer postponed |
|
7 |
FGP_ERR_NOT_ALL_REGISTER_FOUND |
one or both registers cannot be found |