Register Map (Organization of Communication Variables)
Introduction
Communication variables are listed in tables, according to the group (such as identification, statistics, or monitoring) to which they belong. They are associated with an LTMR controller, which may or may not have an LTME expansion module attached.
Communication Variable Groups
Communication variables are grouped according to the following criteria:
|
Variable Groups |
Registers |
|---|---|
|
Identification variables |
00 to 99 |
|
Statistics variables |
100 to 449 |
|
Monitoring variables |
450 to 539 |
|
Configuration variables |
540 to 699 |
|
Command variables |
700 to 799 |
|
User Map variables |
800 to 999 |
|
Custom Logic variables |
1200 to 1399 |
Table Structure
Communication variables are listed in 4-column tables:
|
Column 1 Register (in decimal format) |
Column 2 Variable type Data Types |
Column 3 Variable name and access via Read-only or Read/Write Modbus requests |
Column 4 Note: code for additional information |
Note
The Note column gives a code for additional information.
Variables without a code are available for all hardware configurations, and without functional restrictions.
The code can be:
-
Numerical (1 to 9), for specific hardware combinations
-
Alphabetical (A to Z), for specific system behaviors.
|
If the Note is... |
Then the Variable is... |
|---|---|
|
1 |
Available for the LTMR + LTMEV40 combination |
|
2 |
Always available but with a value equal to 0 if no LTMEV40 is connected |
|
3-9 |
Not used |
|
If the Note is... |
Then... |
|---|---|
|
A |
The variable can be written only when the motor is OFF* |
|
B |
The variable can be written only in configuration mode (for example, static characteristics)* |
|
C |
The variable can be written only with no trip* |
|
D-Z |
Not used |
Unused Addresses
Unused addresses fall into three categories:
-
Not significant, in Read-only tables, means that you should ignore the value read whether equal to 0 or not.
-
Reserved, in Read/Write tables, means that you must write 0 in these variables.
-
Forbidden, means that read or write requests are rejected, that these addresses are not accessible at all.