Identification Variables
Identification Variables
Identification variables are described in the following table.
|
Register |
Variable Type |
Read-only Variables |
|
|---|---|---|---|
|
0-34 |
(Not significant) |
||
|
35-40 |
Word[6] |
Expansion commercial reference DT_CommercialReference |
1 |
|
41-45 |
Word[5] |
Expansion serial number |
1 |
|
46 |
UInt |
Expansion ID code |
|
|
47 |
UInt |
Expansion firmware version DT_FirmwareVersion |
1 |
|
48 |
UInt |
Expansion compatibility code |
1 |
|
49-60 |
(Not significant) |
||
|
61 |
Ulnt |
Network port ID code |
|
|
62 |
Ulnt |
Network port firmware version DT_FirmwareVersion |
|
|
63 |
Ulnt |
Network port compatibility code |
|
|
64-69 |
Word[6] |
Controller commercial reference DT_CommercialReference |
|
|
70-74 |
Word[5] |
Controller serial number |
|
|
75 |
Ulnt |
Controller ID code |
|
|
76 |
Ulnt |
Controller firmware version DT_FirmwareVersion |
|
|
77 |
Ulnt |
Controller compatibility code |
|
|
78 |
Ulnt |
Current scale ratio (0.1%) |
|
|
79 |
Ulnt |
Current sensor max |
|
|
80 |
(Not significant) |
|
|
|
81 |
Ulnt |
Current range max (x 0.1 A) |
|
|
82-94 |
(Not significant) |
||
|
95 |
Ulnt |
Load CT ratio (x 0.1 A) |
|
|
96 |
Ulnt |
Maximum Full Load Current (FLC) range (x 0.1 A) |
|
|
97-99 |
(Forbidden) |