Cyclic Data Description
Introduction
The tables below describe the different cyclic data types in byte format and word format (little endian and big endian):
-
Status: input data
-
Command: output data
-
PKW IN: input data (available only in word format)
-
PKW OUT: output data (available only in word format)
Cyclic Data in Byte Format
Cyclic data types in byte format are:
-
Status: input data
-
Command: output data
Status input data in byte format: Input 0 to Input 9
|
Position |
Description |
|---|---|
|
Input 0.0 Run Reverse |
The main circuit contacts are closed. |
|
Input 0.1 Off |
Indication that the device is in the OFF state. |
|
Input 0.2 Run Forward |
The main circuit contacts are closed. |
|
Input 0.3 Thermal Overload Alarm |
An overload alarm condition exists. (461.3) |
|
Input 0.4 Lockout Time |
Communication status register high byte (456.4) |
|
Input 0.5 Auto Mode |
Indication to a remote host controller that the RUN FORWARD, RUN REVERSE and STOP commands will or will not be accepted. 0 = LOCAL CONTROL 1 = AUTO MODE |
|
Input 0.6 System Trip |
A trip condition exists. (455.2) |
|
Input 0.7 System Alarm |
An alarm condition exists. (455.3) |
|
Input 1.0 to 1.3 Reserved |
Reserved |
|
Input 1.4 System Ready |
Ready (455.0) |
|
Input 1.5 Motor Ramping |
Motor ramping: start in progress (455.15) |
|
Input 1.6 Motor Running |
Motor running: current > 20% FLC Min (455.7) |
|
Input 1.7 System tripped |
System tripped (455.4) |
|
Input 2 |
Iav average current - MSB |
|
Input 3 |
Iav average current - LSB |
|
Input 4 Logic Inputs 9-16 of expansion module |
Logic inputs status High byte (457.8-15) |
|
Input 5 Logic Inputs 1-6 of LTMR controller + inputs 7-8 of expansion module |
Logic inputs status Low byte (457.0-7) |
|
Input 6 Reserved |
Logic outputs status High byte (458.8-9) (458.10-15 are not significant) |
|
Input 7 Status of logic outputs 13, 23, 33, and 95 |
Logic outputs status Low byte (458.0-3) (458.4-7 are not significant) |
|
Input 8 (456.8) Network port comm loss (456.9) Motor lockout (456.10-15) Reserved |
System status register 2 High byte (456.8-15) |
|
Input 9 (456.0) Auto reset active (456.1) Reserved (456.2) Controller power cycle requested (456.3) Motor restart time undefined (456.4) Rapid cycle lockout (456.5) Load shedding (456.6) Motor high speed (456.7) HMI port comm loss |
System status register 2 Low byte (456.0-7) |
Command output data in byte format: Output 0 to Output 5
|
Position |
Description |
|---|---|
|
Output 0.0 Run Reverse |
Instructs the starter to energize the motor in the reverse direction. |
|
Output 0.1 Off |
Instructs the device to go to the OFF state. 0 = ENABLE RUN FORWARD/ RUN REVERSE 1 = OFF |
|
Output 0.2 Run Forward |
Instructs the starter to energize the motor in the forward direction. |
|
Output 0.3 Self Test Command |
Instructs the device to initiate an internal test routine within the device. (704.5) |
|
Output 0.4 Clear Thermal Capacity Level Command |
Reset thermal memory Instructs the starter to override any trip condition and allows starting. (705.2) Note: This command inhibits thermal protection. Continued operation with inhibited thermal protection should be limited to applications where immediate restart is vital. By setting this bit to 1, the thermal state of the motor is lost: the thermal protection will no longer protect an already warm motor. |
|
Output 0.5 Reserved |
Reserved |
|
Output 0.6 Trip Reset Command |
Trip reset Instructs the starter to reset all resettable trips (one of the preconditions for READY). (704.3) |
|
Output 0.7 Reserved |
Reserved |
|
Output 1.0 to 1.4 Reserved |
Reserved |
|
Output 1.5 Motor Low Speed Command |
Low speed (704.6) |
|
Output 1.6 to 1.7 Reserved |
Reserved |
|
Output 2 Additional Output |
Analog output (to manage by custom logic, future extension) (706.8-15) |
|
Output 3 Additional Output |
Analog output (to manage by custom logic, future extension) (706.0-7) |
|
Output 4 Additional Output |
Logic outputs command register High byte (700.8-15: Reserved) |
|
Output 5 Additional Output |
Logic outputs command register Low byte (700.0-3: associated to Output 1 to 4 if custom logic manages it) (700.4-15: Reserved) |
Cyclic Data in Word Little Endian Format
Cyclic data types in Word little endian format are:
-
Status: input data
-
PKW IN: input data
-
Command: output data
-
PKW OUT: output data
Status input data in word little endian format: IW 0 to IW 4
|
Word Arrangement |
Byte N° |
|||
|---|---|---|---|---|
|
IW 0 |
MSB |
bit 15 |
System tripped (455.4) |
Input 1 |
|
bit 14 |
Motor running (455.7) |
|||
|
bit 13 |
Motor starting (455.15) |
|||
|
bit 12 |
System ready (455.0) |
|||
|
bit 8 to bit 11 |
Reserved |
|||
|
LSB |
bit 7 |
System alarm (455.3) |
Input 0 |
|
|
bit 6 |
System trip (455.2) |
|||
|
bit 5 |
Auto mode |
|||
|
bit 4 |
Lock out time |
|||
|
bit 3 |
Thermal overload alarm (461.3) |
|||
|
bit 2 |
Run Forward |
|||
|
bit 1 |
Off |
|||
|
bit 0 |
Run Reverse |
|||
|
IW 1 |
MSB |
bit 8 to bit 15 |
IAV average current % FLC LSB 466.0 to 466.7 |
Input 3 |
|
LSB |
bit 0 to bit 7 |
IAV average current % FLC MSB 466.8 to 466.15 |
Input 2 |
|
|
IW 2 |
MSB |
bit 8 to bit 15 |
Logic inputs status LSB 457.0 to 457.7 Inputs 1-6 of controller Inputs 7-8 of expansion module |
Input 5 |
|
LSB |
bit 0 to bit 7 |
Logic inputs status MSB 457.8 to 457.15 Inputs 9-16 of expansion module (11-16 future extension) |
Input 4 |
|
|
IW 3 |
MSB |
bit 12 to bit 15 |
Outputs 5-8 of expansion module (future extension) 458.4 to 458.7 |
Input 7 |
|
bit 11 |
Logic output 95 status (458.3) |
|||
|
bit 10 |
Logic output 33 status (458.2) |
|||
|
bit 9 |
Logic output 23 status (458.1) |
|||
|
bit 8 |
Logic output 13 status (458.0) |
|||
|
LSB |
bit 0 to bit 7 |
Outputs 9-16 of expansion module (future extension) 458.8 to 458.15 |
Input 6 |
|
|
IW 4 |
MSB |
bit 15 |
HMI port comm loss (456.7) |
Input 9 |
|
bit 14 |
Motor high speed (456.6) |
|||
|
bit 13 |
Load shedding (456.5) |
|||
|
bit 12 |
Rapid cycle lockout (456.4) |
|||
|
bit 11 |
Motor restart time undefined (456.3) |
|||
|
bit 10 |
Controller power cycle requested (456.2) |
|||
|
bit 9 |
Reserved (456.1) |
|||
|
bit 8 |
Auto reset active (456.0) |
|||
|
LSB |
bit 2 to bit 7 |
Reserved (456.10 to 456.15) |
Input 8 |
|
|
bit 1 |
Motor transition lockout (456.9) |
|||
|
bit 0 |
Network port comm loss (456.8) |
|||
PKW IN input data in word little endian format: IW 5 to IW 8 (supported by modules with PKW)
|
Word Arrangement |
|||
|---|---|---|---|
|
IW 5 |
MSB |
bit 8 to bit 15 |
Object address MSB |
|
LSB |
bit 0 to bit 7 |
Object address LSB |
|
|
IW 6 |
MSB |
bit 15 |
Toggle bit |
|
bit 8 to bit 14 |
Function |
||
|
LSB |
bit 0 to bit 7 |
Not used: 0x00 |
|
|
IW 7 |
MSB |
bit 8 to bit 15 |
Data read in register 1 MSB |
|
LSB |
bit 0 to bit 7 |
Data read in register 1 LSB |
|
|
IW 8 |
MSB |
bit 8 to bit 15 |
Data read in register 2 MSB |
|
LSB |
bit 0 to bit 7 |
Data read in register 2 LSB |
|
Command output data in word little endian format: QW 0 to QW 2
|
Word Arrangement |
Byte N° |
|||
|---|---|---|---|---|
|
QW 0 |
MSB |
bit 14 to bit 15 |
Reserved |
Output 1 |
|
bit 13 |
Motor low speed command (704.6) |
|||
|
bit 8 to bit 12 |
Reserved |
|||
|
LSB |
bit 7 |
Reserved |
Output 0 |
|
|
bit 6 |
Trip reset command |
|||
|
bit 5 |
Auto mode |
|||
|
bit 4 |
Clear thermal capacity level command (705.2) |
|||
|
bit 3 |
Self test command (704.5) |
|||
|
bit 2 |
Run Forward (704.0) |
|||
|
bit 1 |
OFF |
|||
|
bit 0 |
Run Reverse (704.1) |
|||
|
QW 1 |
MSB |
bit 8 to bit 15 |
Analog output LSB (future extension) 706.0 to 7 |
Output 3 |
|
LSB |
bit 0 to bit 7 |
Analog output MSB (future extension) 706.8 to 15 |
Output 2 |
|
|
QW 2 |
MSB |
bit 9 to bit 15 |
Logic output command register LSB 700.4 to 7 Outputs 5 to 8 (future extension) |
Output 5 |
|
bit 8 to 11 |
Logic output command register LSB 700.0 to 3 Outputs 1 to 4 (13, 23, 33, 95) if custom logic manages it |
|||
|
LSB |
bit 0 to bit 7 |
Logic output command register MSB 700.8 to 15 Outputs 9 to 16 (future extension) |
Output 4 |
|
PKW OUT output data in word little endian format: QW 3 to QW 6 (supported by modules with PKW)
|
Word Arrangement |
|||
|---|---|---|---|
|
QW 3 |
MSB |
bit 8 to bit 15 |
Object address MSB |
|
LSB |
bit 0 to bit 7 |
Object address LSB |
|
|
QW 4 |
MSB |
bit 15 |
Toggle bit |
|
bit 8 to bit 14 |
Function |
||
|
LSB |
bit 0 to bit 7 |
Not used: 0x00 |
|
|
QW 5 |
MSB |
bit 8 to bit 15 |
Data write in register 1 MSB |
|
LSB |
bit 0 to bit 7 |
Data write in register 1 LSB |
|
|
QW 6 |
MSB |
bit 8 to bit 15 |
Data write in register 2 MSB |
|
LSB |
bit 0 to bit 7 |
Data write in register 2 LSB |
|
Cyclic Data in Word Big Endian Format
Cyclic data types in Word big endian format are:
-
Status: input data
-
PKW IN: input data
-
Command: output data
-
PKW OUT: output data
Status input data in word big endian format: IW 0 to IW 4
|
Word Arrangement |
Byte N° |
|||
|---|---|---|---|---|
|
IW 0 |
MSB |
bit 15 |
System alarm (455.3) |
Input 0 |
|
bit 14 |
System trip (455.2) |
|||
|
bit 13 |
Auto mode |
|||
|
bit 12 |
Lock out time |
|||
|
bit 11 |
Thermal overload alarm (461.3) |
|||
|
bit 10 |
Run Forward |
|||
|
bit 9 |
OFF |
|||
|
bit 8 |
Run Reverse |
|||
|
LSB |
bit 7 |
System tripped (455.4) |
Input 1 |
|
|
bit 6 |
Motor running (455.7) |
|||
|
bit 5 |
Motor ramping (455.15) |
|||
|
bit 4 |
System ready (455.0) |
|||
|
bit 0 to 3 |
Reserved |
|||
|
IW 1 |
MSB |
bit 8 to bit 15 |
IAV average current % FLC MSB 466.8 to 466.15 |
Input 2 |
|
LSB |
bit 0 to bit 7 |
IAV average current % FLC LSB 466.0 to 466.7 |
Input 3 |
|
|
IW 2 |
MSB |
bit 8 to bit 15 |
Logic input status MSB 457.8 to 15 Inputs 9-16 of expansion module (11-16 future extension) |
Input 4 |
|
LSB |
bit 0 to bit 7 |
Logic input status LSB 457.0 to 457.7 Inputs 1-6 of controller Inputs 7-8 of expansion module |
Input 5 |
|
|
IW 3 |
MSB |
bit 8 to bit 15 |
Outputs 9-16 of expansion module (future extension) 458.8 to 458.15 |
Input 6 |
|
LSB |
bit 4 to bit 7 |
Outputs 5-8 of expansion module (future extension) 458.4 to 458.7 |
Input 7 |
|
|
bit 3 |
Logic output 95 status (458.3) |
|||
|
bit 2 |
Logic output 33 status (458.2) |
|||
|
bit 1 |
Logic output 23 status (458.1) |
|||
|
bit 0 |
Logic output 13 status (458.0) |
|||
|
IW 4 |
MSB |
bit 10 to bit 15 |
Reserved (456.10 to 456.15) |
Input 8 |
|
bit 9 |
Motor transition lockout (456.9) |
|||
|
bit 8 |
Network port comm loss (456.8) |
|||
|
LSB |
bit 7 |
HMI port comm loss (456.7) |
Input 9 |
|
|
bit 6 |
Motor high speed (456.6) |
|||
|
bit 5 |
Load shedding (456.5) |
|||
|
bit 4 |
Rapid cycle lockout (456.4) |
|||
|
bit 3 |
Motor restart time undefined (456.3) |
|||
|
bit 2 |
Controller power cycle requested (456.2) |
|||
|
bit 1 |
Reserved (456.1) |
|||
|
bit 0 |
Auto reset active (456.0) |
|||
PKW IN input data in word big endian format: IW 5 to IW 8 (supported by modules with PKW)
|
Word Arrangement |
|||
|---|---|---|---|
|
IW 5 |
MSB |
bit 8 to bit 15 |
Object address LSB |
|
LSB |
bit 0 to bit 7 |
Object address MSB |
|
|
IW 6 |
MSB |
bit 8 to bit 15 |
Not used: 0x00 |
|
LSB |
bit 7 |
Toggle bit |
|
|
bit 0 to bit 6 |
Function |
||
|
IW 7 |
MSB |
bit 8 to bit 15 |
Data read in register 1 LSB |
|
LSB |
bit 0 to bit 7 |
Data read in register 1 MSB |
|
|
IW 8 |
MSB |
bit 8 to bit 15 |
Data read in register 2 LSB |
|
LSB |
bit 0 to bit 7 |
Data read in register 2 MSB |
|
Command output data in word big endian format: QW 0 to QW 2
|
Word Arrangement |
Byte N° |
|||
|---|---|---|---|---|
|
QW 0 |
MSB |
bit 15 |
Reserved |
Output 0 |
|
bit 14 |
Trip reset command |
|||
|
bit 13 |
Auto mode |
|||
|
bit 12 |
Clear thermal capacity level command (705.2) |
|||
|
bit 11 |
Self test command (704.5) |
|||
|
bit 10 |
Run Forward (704.0) |
|||
|
bit 9 |
OFF |
|||
|
bit 8 |
Run Reverse (704.1) |
|||
|
LSB |
bit 6 to bit 7 |
Reserved |
Output 1 |
|
|
bit 5 |
Motor low speed command (704.6) |
|||
|
bit 0 to bit 4 |
Reserved |
|||
|
QW 1 |
MSB |
bit 8 to bit 15 |
Analog output MSB (future extension) 706.8 to 15 |
Output 2 |
|
LSB |
bit 0 to bit 7 |
Analog output LSB (future extension) 706.0 to 7 |
Output 3 |
|
|
QW 2 |
MSB |
bit 8 to bit 15 |
Logic output command register MSB 700.8 to 15 Outputs 9 to 16 (future extension) |
Output 4 |
|
LSB |
bit 4 to bit 7 |
Logic output command register LSB 700.4 to 7 Outputs 5 to 8 (future extension) |
Output 5 |
|
|
bit 0 to 3 |
Logic output command register LSB 700.0 to 3 Outputs 1 to 4 (13, 23, 33, 95) if custom logic manages it |
|||
PKW OUT output data in word big endian format: QW 3 to QW 6 (supported by modules with PKW)
|
Word Arrangement |
|||
|---|---|---|---|
|
QW 3 |
MSB |
bit 8 to bit 15 |
Object address LSB |
|
LSB |
bit 0 to bit 7 |
Object address MSB |
|
|
QW 4 |
MSB |
bit 8 to bit 15 |
Not used: 0x00 |
|
LSB |
bit 7 |
Toggle bit |
|
|
bit 0 to bit 6 |
Function |
||
|
QW 5 |
MSB |
bit 8 to bit 15 |
Data write in register 1 LSB |
|
LSB |
bit 0 to bit 7 |
Data write in register 1 MSB |
|
|
QW 6 |
MSB |
bit 8 to bit 15 |
Data write in register 2 LSB |
|
LSB |
bit 0 to bit 7 |
Data write in register 2 MSB |
|