DOCA0131EN-03

DIN rail

A steel mounting rail, made pursuant to DIN standards (typically 35 mm wide) that allows for easier "snap-on" mounting of IEC electrical devices, including the LTMR controller and the expansion module. Contrast with screw mounting of devices to a control panel by drilling and tapping holes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?