Add to Selection

Add to Selection allows you to add the selected feature to the Selection tab. If you right-click a feature layer in the tree (the Fuse layer in the example below) and select Add to Selection, all features under that layer will be added to the Selection tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.