ArcFM Viewer Toolbar

The ArcFM Viewer toolbar provides the user with tools to print, modify, and refresh the map display.

Tool

Description

Print

This tool allows you to modify and print the current map display.

Map Scale

Use this field to modify the scale of the map display.

Refresh View

Click this button to refresh the map display.

Synchronize Map Tabs

Synchronizes all map tabs so that each one shows the same area of the map at all times. If the user changes the display on one tab, all others synchronize to match it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.