Session Redliner - Basic

This implementation allows the field user to place redline graphics with sessions while working in the field. A field editor may create a new redline session or access an existing one in the field, add redline graphics, then send the session to an enterprise user. With this implementation, graphics are saved with the session.

Configuration (refer to Mobile Configuration Guide): Basic Redliner

Required ArcFM Licenses in the Field: Redliner Extension and ArcFM , ArcFM Viewer for ArcGIS Engine, or the ArcFM Viewer that works with ArcGIS for Desktop Basic (formerly ArcView)

Required Esri Licenses in the Field: Engine Runtime or ArcGIS for Desktop Basic

Field Databases: Backdrop, Login (optional), Process Framework (e.g., Session Manager)

In the field, You may choose to use ArcFMArcFM Viewer for ArcGIS Engine, or the ArcFM Viewer that works with ArcGIS for Desktop Basic. Most commonly, ArcFM Viewer for ArcGIS Engine is used because it is a powerful, light-weight solution. The following work flows are examples. Your work flow may vary.

Work Flow Example 1: Redlining Started in the Field

Work Flow Example 2: Redline Sessions Created on Enterprise 

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.