ArcFM Underground Facility Diagrams Toolbar

This toolbar provides the tools to view existing underground facility diagrams.

Tool

Description

Launch Diagram Manager

Use this tool to view an existing diagram and open the Diagram Manager.

Close Diagram Manager

Click this button to dismiss the Diagram Manager window.

Navigate to Next Facility

Click this button, then click a duct bank to navigate to the next underground facility. Use this tool to navigate through the underground facilities network.

Navigate to Previous Facility

Click this button to navigate to the previous underground facility. This button remains disabled until the Navigate to Next Facility button has been used.

Select Diagram

Click this button to select the current underground facility diagram. You may view information about the individual selected features on the Selection tab.

Select Duct Bank

Click this button, then click a duct bank to select it. You may view information about the individual selected features on the Selection tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.