Highlight

You can use the Highlight utility to see a selected feature highlighted (the feature flashes three times) on the map. Use the General tab in ArcFM Viewer Options General tab in ArcFM Viewer Options to modify the size and color of the highlight.

Right-click a feature (or multiple features) and select Highlight to see the feature flash three times on the map. If the selected feature is out of visible range, use Zoom To before using Highlight.

IMPORTANT: If the highlighted feature is hidden behind a form such as the Attribute Viewer or ArcFM Locator, the form window will become transparent to make the highlighted feature visible when it flashes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.