Fiber Trace

The Fiber Trace tool traces a path of connectivity that was previously established with Connection Manager. The trace uses connectivity information at each junction to determine fibers' paths in both directions. This tool is useful for checking the connectivity of a light path between two points in a system. The following sections describe the process for linear tracing and point tracing. 

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.