Fiber Trace

The highlighted row on the report indicates the trace origin. If you use directional tracing, the highlighted row appears at the top of the report. If you do not use directional tracing, the highlighted row can appear any where in the report. This report shows a directional fiber trace:

IMPORTANT: In order to view the Fiber Trace Report in the style shown above, you may need to delete the existing Trace_Report.xsl file from your ...\AppData\Local\Temp directory.The contents of the Additional Information column can be configured by an administrator.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.