Products and Licenses

ArcFM Viewer for ArcGIS Engine and its compatible extensions provide varying levels of editing capabilities. The Redliner and Inspector extensions require ArcFM Viewer with ArcGIS Engine along with its valid licensing. However, these two extensions do not rely upon one another and may be used independently.

 

Capabilities Licenses

Esri Licenses

Capabilities

Capabilities Viewer for ArcGIS Engine

Capabilities Viewer for ArcGIS Engine

Engine Runtime

View and query

Redliner

Capabilities Viewer for ArcGIS Engine, Redliner extension

Engine Runtime

View, query, redline editing

Inspector

Capabilities Viewer for ArcGIS Engine, Engine Editor extension

Engine Runtime

View, query, redline editing, and non-spatial attribute editing

Engine runtime, Geodatabase Update extension

View, query, redline editing, and attribute editing for various types* of features

* A Geodatabase Update Extension license is required from Esri in order to edit relationship classes, feature-linked annotation, dimension feature classes and custom feature classes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.