GPS Support Toolbar

The GPS Support toolbar provides access to tools that let you interact with your GPS and display GPS points on the map display.

Tool

Description

GPS Connection Setup

Set connection parameters for a GPS receiver.

Clear GPS Display

Clears all GPS symbology displayed on the map.

Display Options

Allows you to determine the color of the GPS display symbology. Click the colored box (it shows the current selection) to display a color picker. Choose a color and select OK. Click OK on the Display Options dialog to save the change.

Open Connection

Opens a connection to the GPS receiver.

Close Connection

Closes the connection to the GPS receiver.

Auto Pan

When this button is toggled ON, the tool automatically pans to each GPS point. This tool automatically zooms to the first point when GPS connection is opened.

Zoom To

Zooms to the current GPS point.

Rotate

When this button is toggled ON, the tool automatically rotates the map so the direction of each GPS location is facing "up" in the map display. This button may only be toggled ON if the Auto Pan button is also ON.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.