Pan To

This right-click utility allows you to refocus the display to include the selected feature(s) without changing the scale. Pan To may be used with multiple features. However, all of the selected features may not appear in the display if the scale doesn't allow.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.