Digital Ink and Gestures

For tablet PC users, ArcFM Viewer provides tools to use Digital Ink and gestures. All of these tools are available on the Tablet toolbar and allow the user to draw on a tablet PC using a stylus.

While you may use the Ink tool in ArcFM Viewer for ArcGIS Engine, you must have the Redliner extension or the Inspector extension in order to save these redline marks to a session. Otherwise, they are not saved. Gestures are supported on a tablet PC both with and without the Redliner or Inspector extensions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.