De-Energized Features

Generally, electrical features that remain de-energized in a normal switching state represent a data problem, usually in the form of a switchable device that is incorrectly attributed as “open” on one or more phases. This search allows you to locate any de-energized features in the network.

  1. Select the Locate Lines Only checkbox to view only conductor features.
  2. Select the Auto Zoom To Select checkbox if you want to zoom the display to the selected feeder(s) when the search is complete.
  3. Choose a Substation.
  4. Select a feeder from the grid.
  5. Click Apply.
  6. Click the Stop button if you want to end the search before it is complete.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.