Redlining Started in the Field

This work flow assumes that no redline sessions are created on the enterprise, and the editor begins the redline session in the field. This work flow is most common and provides the simplest solution.

  • Start Redlining: Click the Open New Redline Session button on the Session Manager toolbar in ArcFM Viewer (the session is created and opened in ArcFM Viewer).

  • Navigate/Query Map: While using ArcFM Viewer for ArcGIS Engine or ArcFM Viewer (Desktop) in the field, all ArcFM Viewer tools (e.g., Locator, Identify, Tracing) are available to the user. 

  • Place Graphics: Place graphics on the map using the Graphics tab. Save and close session when finished. Graphics are stored with the session.

  • Digital Ink and Gestures (ArcFM Engine Only): The Digital Ink and Gestures tools available in ArcFM Viewer for ArcGIS Engine are also available with Redliner (only if you're using Redliner on ArcFM Viewer for ArcGIS Engine).

  • Send Redlines: There are two options for sending your redline edits to the Enterprise. The first option is the easiest and most commonly used.

    1. Use the Send Session task or button to select a user and send the session to the enterprise.

    2. Use the Send Session to Enterprise task to submit the graphic session to an enterprise user.

  • Send/Receive Mobile Data (optional): If your administrator has configured Geodatabase Replication to automatically send and receive sessions, this step is not necessary. Otherwise, execute the Send/Receive Mobile Data task to send data to the enterprise (and retrieve any data sent from the enterprise). This final task requires a network connection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.