Underground Facility Manager

The Underground Facility Manager (UFM) allows you to view underground structures and navigate the underground facilities network. The Underground Facility Diagrams toolbar offers navigation tools as well as buttons that allow you to select the diagram or a duct bank. Underground structure features (e.g., walls, floor, duct banks) are visible only if they have been placed on the map. These features are created using Conduit Manager in ArcFM .

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.