Multiple Map Display Tabs

You may have multiple stored displays visible on multiple tabs. Use the Add New Tab tool to create additional map display tabs. Select the newly created tab and then choose a stored display to populate it with data.

Using the right-click tools on the map display tab, you can arrange tabs vertically or horizontally.

IMPORTANT: These changes are not persisted when you close ArcFM Viewer. Each time the user opens the application, only a single tab is available until the user creates a horizontal or vertical group

Horizontal display

Vertical display

Use the Synchronize Map Tabs tool to display the same area on every Map Display tab. 

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.