Patch Panel Connection Report

A patch panel connection report is a graphical display of the layout of a patch panel or a series of patch panels. This section describes the steps used in creating a patch panel connection report.

  1. Click the Patch Panel Connection Report button on the Fiber Viewer toolbar.
  2. Use the flag cursor  to select the patch location containing the patch panel on which you want to create a report.
  3. One of two windows appears.
    IMPORTANT: Fiber Viewer works with both the ArcFM Solutions classic data model and the flexible data model. If you are working with the classic data model, the Patch Panels window appears. If you are working with the flexible data model, the Select report item window appears.

    Patch Panel Report for the Flexible Data Model

    Classic Patch Panel Report

     

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.