Add Toolbar to User Interface

If a toolbar is missing from your ArcFM Engine application (e.g., ArcFM Viewer), you may restore it to the user interface using a couple different methods.

  1. Right-click the area around the toolbars.
  2. Select the toolbar from the list. If a checkmark appears next to the toolbar, it is already in the display.

     

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.