Select by Feeder

This tool allows you to identify and highlight a feeder or set of feeders on a map. The selected features on the feeder system will be highlighted in blue on your map. The features will also be available on the Selection tab of the Attribute Editor.

  1. From the Selection menu, choose Select by Feeder.
  2. In the Select by Feeders dialog box, select the types of features you want to search for.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.