Attribute Viewer Tab

The Attribute Viewer tab allows you to modify various settings for the Selection tab in ArcFM Viewer for ArcGIS Engine.

  • Layer Order: You may determine the order in which features appear on the Selection tab. Choose from drawing order or alphabetical order.

  • Automatically Expand Selection Tab: This option expands and selects the top node in the list when features are added to the Selection tab of the Attribute Viewer.

    • Never: This option is disabled. When features are added to the Selection tab, they remain collapsed until the user expands them.

    • When a single feature is selected: When a single feature is added to the Selection tab (or multiple features in the same feature class), it is expanded and selected so its attributes are shown in the grid on the Selection tab.

    • Always: The top feature in the list is expanded and selected regardless of the number of features selected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.