Switchable Device Network Categories

Unbalanced Network

​The following attributes exist on both the Device feature class and the JunctionObject table in the electric domain network. They are common in and may be populated for any of the subclasses of switchable devices, such as fuses and reclosers.

Name 

Data Type 

Description 

Sample Data 

​DeviceStatus 

Short or Long ​Integer

​Open/Closed state of the device (N/A for banks).  Open, Traceable allows for features to be owned by the subnetwork for things like export subnetwork but have no energized phases.  

​0 = Open 

​1 = Closed

​2 = Open, Traceable 

​RatedCurrent 

Short or Long ​Integer

​Current rating in amps. 

 

​MaxInterruptingAmps 

Short or Long ​Integer

​Maximum current in amps that the device can safely interrupt. 

 

​MaxOperatingVolts 

Short or Long ​Integer

​Voltage rating in volts. 

 

Is​GangOperated 

Short or Long ​Integer

​Used to note in the unbalanced model if a switchable device is gang operated. 

​1-Yes 

​0-No 


Balanced Network Requirements

​The DeviceStatus and PhasesNormal attributes are required for all switchable device unit records in the JunctionObject table and Electric Device Feature Class. ​The following attributes only exist on the device feature class. They are common in the sense that they may be populated (though not required to be populated) for any of the subclasses of switchable device, such as fuses and reclosers.

Name 

Data Type 

Description 

Sample Data 

​DeviceStatus 

Short or Long ​Integer

​Open/Closed state of the device (N/A for banks).  Open, traceable allows for features to be owned by the subnetwork for things like export subnetwork but have no energized phases.  

​0 = Open 

​1 = Closed 

​2= Open, Traceable

​RatedCurrent 

Short or Long ​Integer

​Current rating in amps. 

 

​MaxInterruptingAmps 

Short or Long ​Integer

​Maximum current in amps that the device can safely interrupt. 

 

​MaxOperatingVolts 

Short or Long ​Integer

​Voltage rating in volts. 

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.