Device Controllers
Device controllers work with the protection and control system to automatically turn distribution equipment on and off as needed to maintain grid stability. Controllers provide precise, unvaried operation based on real-time data and analytics and are customized to unique requirements.
Device Controller in Network Categories
|
Equipment Type |
Network Category |
Applicable tables |
Description |
|---|---|---|---|
|
Device Controller |
E:Device Controller |
ElectricJunctionObject |
Applies to a JunctionObject Record that can be contained by another JunctionObject Record representing the Unit has a Device Controller. |
Device Controller in Unbalanced Model
Device Controller in Balanced Model with Disconnected Units
Required Configurations
-
Must model with units using either E:Has Connected Units or E:Has Disconnected Units.
-
The device controllers are records in the electric JunctionObject table.
-
The device controllers will be contained by the Unit they control.
-
The device controller asset group asset type must have the E:Device Controller network category applied.