Network Modeling Categories
The Modeling Categories are used to discriminate features according to essential properties of interest to certain applications. Some of these have to do with specific modeling capabilities of the Utility Network (UN) data model and indicate a choice in the way the ArcFM UN leverages those capabilities. The Tap Transformer, Inline Transformer, and Units Required categories are a few example categories. Other categories in this group help classify equipment using another property. The categories Overhead, Underground, and Submersible for example, all give a hint about the expected operating environment and design of the equipment to which they attach.
|
Network Category Name |
Applicable tables |
Description |
|---|---|---|
|
E:Conductor Info |
EdgeObject |
Used to identify non-spatial edge records that represent Conductor Info objects |
|
E:Overhead |
Line EdgeObject Device |
Used to denote which conductors or transformers are installed on overhead poles |
|
E:Has Connected Units |
ElectricDevice |
Used to identify a two-terminal feature type that serves as an electrical bank that contains non-spatial phase-specific units. Non-membership in this category indicates that the feature type is not allowed to have units. |
|
E:Unit |
JunctionObject |
Used to tell the difference between a non-spatial junction that represents a unit, in the bank/unit containment pattern, and one that does not. |
|
E:Open Point |
JunctionObject |
Used to identify a non-spatial unit (of a switchable device) whose DeviceStatus is permanently stuck in the “Open” state. |
|
E:Pass Through |
JunctionObject |
Used to identify a non-spatial unit, of a switchable device, whose DeviceStatus is permanently stuck in the closed state. |
|
E:Protective |
Device JunctionObject |
This category is used to form Conditions in Trace Configurations that need to identify protective devices, such as a Protective Device Trace. |
|
E:Transformer – Tap |
Device JunctionObject |
Transformers with this network category are connected to the network through a TransformerTap. |
|
E:Transformer - Inline |
Device JunctionObject |
Transformers with this network category can only be connected at endpoints of conductors. |
|
E:Submersible |
Line EdgeObject Device |
Used to denote which conductors or transformers or switches, etc. are designed for underwater connections. |
|
E:Underground |
Line EdgeObject Device |
Used to denote which conductors or transformers or switches, etc. are installed in underground structural networks. |
|
E:Composite Electric Equipment |
Assembly StructureBoundary |
Denotes a high-order electric entity, such as a switch cabinet or a substation bay, that is a grouping of multiple features in the electric domain network, such as switches, fuses, busbar, conductors, etc. |
|
E:Has Functional Equipment (Balanced Model Only) |
Electric Device |
Any electric device that could have functional equipment in the non-spatial object tables. |
|
E:Functional Equipment (Balanced Model Only) |
Junction Object |
Non-spatial objects that can be functional equipment |